<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32VのトピックS32V: SRC_GPR Registers: Write failures?</title>
    <link>https://community.nxp.com/t5/S32V/S32V-SRC-GPR-Registers-Write-failures/m-p/734691#M94</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV class=""&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm trying to configure the PCIE related registers on the S32v EVB board and I keep encountering strange behaviour.&lt;/P&gt;&lt;P&gt;For example, once QNX is up and running on the S32V EVB board, I tried reading the SRC_GPR5 register (address: 0x4007C110). The read succeeded and I got the following value -- 0x12500208 .&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, if I try to write to this register after the OS has booted, I get a bus error.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can easily configure this registers in IPL and u-boot. I can't seem to do it after QNX is up and running. I've checked that the register itself is R/W and is a non-secure register (based on the TRM).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can someone let me know if the TRM was updated or there is anything special I need to do to write to these registers once the OS is up and running?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ekta&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Feb 2018 19:04:44 GMT</pubDate>
    <dc:creator>ektasachdev</dc:creator>
    <dc:date>2018-02-09T19:04:44Z</dc:date>
    <item>
      <title>S32V: SRC_GPR Registers: Write failures?</title>
      <link>https://community.nxp.com/t5/S32V/S32V-SRC-GPR-Registers-Write-failures/m-p/734691#M94</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV class=""&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm trying to configure the PCIE related registers on the S32v EVB board and I keep encountering strange behaviour.&lt;/P&gt;&lt;P&gt;For example, once QNX is up and running on the S32V EVB board, I tried reading the SRC_GPR5 register (address: 0x4007C110). The read succeeded and I got the following value -- 0x12500208 .&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, if I try to write to this register after the OS has booted, I get a bus error.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can easily configure this registers in IPL and u-boot. I can't seem to do it after QNX is up and running. I've checked that the register itself is R/W and is a non-secure register (based on the TRM).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can someone let me know if the TRM was updated or there is anything special I need to do to write to these registers once the OS is up and running?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ekta&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Feb 2018 19:04:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32V/S32V-SRC-GPR-Registers-Write-failures/m-p/734691#M94</guid>
      <dc:creator>ektasachdev</dc:creator>
      <dc:date>2018-02-09T19:04:44Z</dc:date>
    </item>
    <item>
      <title>Re: S32V: SRC_GPR Registers: Write failures?</title>
      <link>https://community.nxp.com/t5/S32V/S32V-SRC-GPR-Registers-Write-failures/m-p/734692#M95</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ekta,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From your question, it seems that it is some prevention mechanism in QNX OS that is preventing access to this register.&lt;/P&gt;&lt;P&gt;I will recommend to contact QNX for support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kushal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Apr 2018 17:25:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32V/S32V-SRC-GPR-Registers-Write-failures/m-p/734692#M95</guid>
      <dc:creator>KushalShahNXP</dc:creator>
      <dc:date>2018-04-30T17:25:52Z</dc:date>
    </item>
  </channel>
</rss>