<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic APECV gftt corner detector error in S32V</title>
    <link>https://community.nxp.com/t5/S32V/APECV-gftt-corner-detector-error/m-p/729225#M78</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am currently trying to use good feature to track corner detector from apexcv in one of my project. I was able to call Initilize() and Process() function without error code return (these functions always return 0). However inside the Process() function, i got the following message:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ACF_PROCESS_APU::SelectScenario_internal() -&amp;gt; A suitable scenario could not be found&lt;/P&gt;&lt;P&gt;ACF_PROCESS_APU::Wait() -&amp;gt; process was never started (i.e. nothing to wait for)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After reading the source code of acf_process_apu, its appear that this error is related to the setting of chunkWidth and chunkHeight. However, i did not see any function that allow me to configure them.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The input image is a gray scale image with size 1280x800. I also tried different image size, but they are all returning same error message.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Jan 2018 18:12:28 GMT</pubDate>
    <dc:creator>xuewong</dc:creator>
    <dc:date>2018-01-16T18:12:28Z</dc:date>
    <item>
      <title>APECV gftt corner detector error</title>
      <link>https://community.nxp.com/t5/S32V/APECV-gftt-corner-detector-error/m-p/729225#M78</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am currently trying to use good feature to track corner detector from apexcv in one of my project. I was able to call Initilize() and Process() function without error code return (these functions always return 0). However inside the Process() function, i got the following message:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ACF_PROCESS_APU::SelectScenario_internal() -&amp;gt; A suitable scenario could not be found&lt;/P&gt;&lt;P&gt;ACF_PROCESS_APU::Wait() -&amp;gt; process was never started (i.e. nothing to wait for)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After reading the source code of acf_process_apu, its appear that this error is related to the setting of chunkWidth and chunkHeight. However, i did not see any function that allow me to configure them.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The input image is a gray scale image with size 1280x800. I also tried different image size, but they are all returning same error message.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jan 2018 18:12:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32V/APECV-gftt-corner-detector-error/m-p/729225#M78</guid>
      <dc:creator>xuewong</dc:creator>
      <dc:date>2018-01-16T18:12:28Z</dc:date>
    </item>
    <item>
      <title>Re: APECV gftt corner detector error</title>
      <link>https://community.nxp.com/t5/S32V/APECV-gftt-corner-detector-error/m-p/729226#M79</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xue,&lt;/P&gt;&lt;P&gt;Please raise the ticket at &lt;A href="http://www.nxp.com/suport"&gt;www.nxp.com/suport&lt;/A&gt;&amp;nbsp;using "Service Request" for support on this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Kushal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Apr 2018 20:42:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32V/APECV-gftt-corner-detector-error/m-p/729226#M79</guid>
      <dc:creator>KushalShahNXP</dc:creator>
      <dc:date>2018-04-30T20:42:44Z</dc:date>
    </item>
  </channel>
</rss>