<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32VのトピックRe: S32DS_ARM_Linux_v1.3.bin Install: No Java VM could be found from PATH.</title>
    <link>https://community.nxp.com/t5/S32V/S32DS-ARM-Linux-v1-3-bin-Install-No-Java-VM-could-be-found-from/m-p/672218#M25</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had the same issue. Try installing java 1.8 and see if this resolves the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This solution also seems to be at odds with the latest Yocto release installation which specifically requests openjdk-7.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 Sep 2017 14:32:17 GMT</pubDate>
    <dc:creator>davidewing</dc:creator>
    <dc:date>2017-09-22T14:32:17Z</dc:date>
    <item>
      <title>S32DS_ARM_Linux_v1.3.bin Install: No Java VM could be found from PATH.</title>
      <link>https://community.nxp.com/t5/S32V/S32DS-ARM-Linux-v1-3-bin-Install-No-Java-VM-could-be-found-from/m-p/672216#M23</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;Hi,when I install S32DS_ARM_Linux_v1.3.bin in ubuntu 14.04, I got messege in shell:&lt;/P&gt;&lt;P&gt;Preparing to install...&lt;/P&gt;&lt;P&gt;Extracting the installation resources from the installer archive...&lt;/P&gt;&lt;P&gt;Configuring the installer for this system's environment...&lt;/P&gt;&lt;P&gt;No Java virtual machine could be found from your PATH environment variable. &amp;nbsp;You must install a VM prior to running this program.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I have installed java and java version is:&lt;/P&gt;&lt;P&gt;user@ubuntu:~$ java -version&lt;/P&gt;&lt;P&gt;java version "1.7.0_80"&lt;/P&gt;&lt;P&gt;Java(TM) SE Runtime Environment (build 1.7.0_80-b15)&lt;/P&gt;&lt;P&gt;Java HotSpot(TM) 64-Bit Server VM (build 24.80-b11, mixed mode).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also I have set necessary &amp;nbsp;environment variables in .bashrc:&lt;/P&gt;&lt;P&gt;export JAVA_HOME=/usr/lib/jvm/jdk1.7.0_80&lt;/P&gt;&lt;P&gt;export JRE_HOME=${JAVA_HOME}/jre&lt;/P&gt;&lt;P&gt;export CLASSPATH=.:${JAVA_HOME}/lib:${JRE_HOME}/lib &amp;nbsp;&lt;/P&gt;&lt;P&gt;export PATH=${JAVA_HOME}/bin:${JRE_HOME}:${CLASSPATH}:$PATH&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are any other &lt;SPAN&gt;environment variables&lt;/SPAN&gt; that I didn't set or I should add some path in PATH? Or the jre version is not correct?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 25 Jun 2017 02:15:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32V/S32DS-ARM-Linux-v1-3-bin-Install-No-Java-VM-could-be-found-from/m-p/672216#M23</guid>
      <dc:creator>gaomingliang</dc:creator>
      <dc:date>2017-06-25T02:15:41Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS_ARM_Linux_v1.3.bin Install: No Java VM could be found from PATH.</title>
      <link>https://community.nxp.com/t5/S32V/S32DS-ARM-Linux-v1-3-bin-Install-No-Java-VM-could-be-found-from/m-p/672217#M24</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the same issue. My environment is&lt;/P&gt;&lt;P&gt;fchen2@T420:~/NXP$ cat /etc/lsb-release&lt;/P&gt;&lt;P&gt;DISTRIB_ID=Ubuntu&lt;BR /&gt;DISTRIB_RELEASE=16.04&lt;BR /&gt;DISTRIB_CODENAME=xenial&lt;BR /&gt;DISTRIB_DESCRIPTION="Ubuntu 16.04.3 LTS"&lt;/P&gt;&lt;P&gt;fchen2@T420:~/NXP$ uname -a&lt;BR /&gt;Linux T420 4.10.0-33-generic #37~16.04.1-Ubuntu SMP Fri Aug 11 14:07:24 UTC 2017 x86_64 x86_64 x86_64 GNU/Linux&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Sep 2017 14:24:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32V/S32DS-ARM-Linux-v1-3-bin-Install-No-Java-VM-could-be-found-from/m-p/672217#M24</guid>
      <dc:creator>fchen2</dc:creator>
      <dc:date>2017-09-19T14:24:18Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS_ARM_Linux_v1.3.bin Install: No Java VM could be found from PATH.</title>
      <link>https://community.nxp.com/t5/S32V/S32DS-ARM-Linux-v1-3-bin-Install-No-Java-VM-could-be-found-from/m-p/672218#M25</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had the same issue. Try installing java 1.8 and see if this resolves the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This solution also seems to be at odds with the latest Yocto release installation which specifically requests openjdk-7.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Sep 2017 14:32:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32V/S32DS-ARM-Linux-v1-3-bin-Install-No-Java-VM-could-be-found-from/m-p/672218#M25</guid>
      <dc:creator>davidewing</dc:creator>
      <dc:date>2017-09-22T14:32:17Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS_ARM_Linux_v1.3.bin Install: No Java VM could be found from PATH.</title>
      <link>https://community.nxp.com/t5/S32V/S32DS-ARM-Linux-v1-3-bin-Install-No-Java-VM-could-be-found-from/m-p/672219#M26</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Same problem here trying to install the PowerPC version on Linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I downloaded the latest 64bit Oracle Java, changed the symlinks in /usr/bin so that /usr/bin/java points to /usr/java/jre1.8.0_144/bin/java&lt;/P&gt;&lt;P&gt;Checked:&lt;BR /&gt;# java -version&lt;BR /&gt;java version "1.8.0_144"&lt;BR /&gt;Java(TM) SE Runtime Environment (build 1.8.0_144-b01)&lt;BR /&gt;Java HotSpot(TM) 64-Bit Server VM (build 25.144-b01, mixed mode)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now the installer runs ok. (I'm sure the earlier installer worked as-is on my system?)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;James&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Sep 2017 09:06:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32V/S32DS-ARM-Linux-v1-3-bin-Install-No-Java-VM-could-be-found-from/m-p/672219#M26</guid>
      <dc:creator>jamesmurray</dc:creator>
      <dc:date>2017-09-28T09:06:58Z</dc:date>
    </item>
  </channel>
</rss>