<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic emmc can't be formatted in S32V</title>
    <link>https://community.nxp.com/t5/S32V/emmc-can-t-be-formatted/m-p/823826#M177</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have developed a platform using S32V234 as the main controller, and have made many boards,among them there are some emmc can't be formatted. There is a 32G emmc(MTFC32GAKAEEF-AIT) per board. the process is, first run u-boot,then run nfsboot,I can login,then run fdisk,the partition table can be printed,&amp;nbsp;the first partition starts at 2048 ends at 524287,Size 255M,Id c, Type W95 FAT32(LBA),and then run mkfs.vfat -n boot /dev/mmcblk0p1,it suspends.&lt;/P&gt;&lt;P&gt;I have tried to change the start position of the first partition and have checked the partition table has changed,but it still can't be formatted.&lt;/P&gt;&lt;P&gt;What can I do except change&amp;nbsp;a new eMMC chip?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Dec 2018 03:47:10 GMT</pubDate>
    <dc:creator>sybilmao</dc:creator>
    <dc:date>2018-12-21T03:47:10Z</dc:date>
    <item>
      <title>emmc can't be formatted</title>
      <link>https://community.nxp.com/t5/S32V/emmc-can-t-be-formatted/m-p/823826#M177</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have developed a platform using S32V234 as the main controller, and have made many boards,among them there are some emmc can't be formatted. There is a 32G emmc(MTFC32GAKAEEF-AIT) per board. the process is, first run u-boot,then run nfsboot,I can login,then run fdisk,the partition table can be printed,&amp;nbsp;the first partition starts at 2048 ends at 524287,Size 255M,Id c, Type W95 FAT32(LBA),and then run mkfs.vfat -n boot /dev/mmcblk0p1,it suspends.&lt;/P&gt;&lt;P&gt;I have tried to change the start position of the first partition and have checked the partition table has changed,but it still can't be formatted.&lt;/P&gt;&lt;P&gt;What can I do except change&amp;nbsp;a new eMMC chip?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Dec 2018 03:47:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32V/emmc-can-t-be-formatted/m-p/823826#M177</guid>
      <dc:creator>sybilmao</dc:creator>
      <dc:date>2018-12-21T03:47:10Z</dc:date>
    </item>
    <item>
      <title>Re: emmc can't be formatted</title>
      <link>https://community.nxp.com/t5/S32V/emmc-can-t-be-formatted/m-p/823827#M178</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;there is howto document related to eMMC, but I'm not sure if it covers your issue ( not tested with SBC board ) . But you can try it -&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-340293"&gt;https://community.nxp.com/docs/DOC-340293&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Dec 2018 19:02:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32V/emmc-can-t-be-formatted/m-p/823827#M178</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2018-12-29T19:02:27Z</dc:date>
    </item>
  </channel>
</rss>