<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Which interface(s) can I use to program the eMMC ? in S32V</title>
    <link>https://community.nxp.com/t5/S32V/Which-interface-s-can-I-use-to-program-the-eMMC/m-p/769747#M155</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm planning to use S32V234 and boot from eMMC. However, which interface or interfaces can I use to program the eMMC? Is it JTAG or some other interface?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Feb 2018 22:13:23 GMT</pubDate>
    <dc:creator>tomlowdermilk</dc:creator>
    <dc:date>2018-02-23T22:13:23Z</dc:date>
    <item>
      <title>Which interface(s) can I use to program the eMMC ?</title>
      <link>https://community.nxp.com/t5/S32V/Which-interface-s-can-I-use-to-program-the-eMMC/m-p/769747#M155</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm planning to use S32V234 and boot from eMMC. However, which interface or interfaces can I use to program the eMMC? Is it JTAG or some other interface?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Feb 2018 22:13:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32V/Which-interface-s-can-I-use-to-program-the-eMMC/m-p/769747#M155</guid>
      <dc:creator>tomlowdermilk</dc:creator>
      <dc:date>2018-02-23T22:13:23Z</dc:date>
    </item>
    <item>
      <title>Re: Which interface(s) can I use to program the eMMC ?</title>
      <link>https://community.nxp.com/t5/S32V/Which-interface-s-can-I-use-to-program-the-eMMC/m-p/769748#M156</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tim,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One of the methods can be loading via network.&lt;/P&gt;&lt;P&gt;Please follow the steps described in&amp;nbsp;&lt;STRONG&gt;Section&amp;nbsp;3.1.2 Setup eMMC memory&lt;/STRONG&gt; of &lt;STRONG&gt;Linux BSP Reference manual&lt;/STRONG&gt; for detailed instructions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kushal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Apr 2018 17:40:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32V/Which-interface-s-can-I-use-to-program-the-eMMC/m-p/769748#M156</guid>
      <dc:creator>KushalShahNXP</dc:creator>
      <dc:date>2018-04-30T17:40:19Z</dc:date>
    </item>
  </channel>
</rss>