<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FlexCAN 64 bits data transmission in S32 SDK</title>
    <link>https://community.nxp.com/t5/S32-SDK/FlexCAN-64-bits-data-transmission/m-p/881567#M919</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to send 64 bit data on CAN.&lt;/P&gt;&lt;P&gt;As of now, I'm successfully able to send 8 bits over CAN&amp;nbsp;&lt;/P&gt;&lt;P&gt;(a) What is the difference between message box and message buffers?&lt;/P&gt;&lt;P&gt;(b) What are the changes in MBs or FIFOs that has to be made so as to send 64 bits data over CAN?&lt;/P&gt;&lt;P&gt;(c) What is the change in the Rx code that has to be made,so as to receive all messages irrespective of IDs and data size?&lt;/P&gt;&lt;P&gt;(d)What are the extra functions that has to be added to the code ( Tn and Rx) to send and receive 64 bits data?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have attached the CAN Rx and Tx files, Do go through it and tell me the changes that I have to make.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CAN_COMM is the transmitter code and CAN_Rx is the receiver code&lt;/P&gt;&lt;P&gt;The images prints the ID and the messages received over the data line.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 04 Feb 2019 07:39:17 GMT</pubDate>
    <dc:creator>sushma</dc:creator>
    <dc:date>2019-02-04T07:39:17Z</dc:date>
    <item>
      <title>FlexCAN 64 bits data transmission</title>
      <link>https://community.nxp.com/t5/S32-SDK/FlexCAN-64-bits-data-transmission/m-p/881567#M919</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to send 64 bit data on CAN.&lt;/P&gt;&lt;P&gt;As of now, I'm successfully able to send 8 bits over CAN&amp;nbsp;&lt;/P&gt;&lt;P&gt;(a) What is the difference between message box and message buffers?&lt;/P&gt;&lt;P&gt;(b) What are the changes in MBs or FIFOs that has to be made so as to send 64 bits data over CAN?&lt;/P&gt;&lt;P&gt;(c) What is the change in the Rx code that has to be made,so as to receive all messages irrespective of IDs and data size?&lt;/P&gt;&lt;P&gt;(d)What are the extra functions that has to be added to the code ( Tn and Rx) to send and receive 64 bits data?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have attached the CAN Rx and Tx files, Do go through it and tell me the changes that I have to make.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CAN_COMM is the transmitter code and CAN_Rx is the receiver code&lt;/P&gt;&lt;P&gt;The images prints the ID and the messages received over the data line.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Feb 2019 07:39:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/FlexCAN-64-bits-data-transmission/m-p/881567#M919</guid>
      <dc:creator>sushma</dc:creator>
      <dc:date>2019-02-04T07:39:17Z</dc:date>
    </item>
  </channel>
</rss>