<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 SDKのトピックRe: CAN interface Demo is needed</title>
    <link>https://community.nxp.com/t5/S32-SDK/CAN-interface-Demo-is-needed/m-p/854252#M768</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually there is a FlexCAN example available. It's based on s32V234 SDK v0.8.1 (EAR) that is currently part of S32DS for S32 Platform only.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-342447"&gt;S32 Design Studio 2018.R1 for S32 Automotive ARM Platform (Windows/Linux) released!&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd recommend you to install this version + S32V2xx development package as described in the release announcement. It can coexist with S32DS for Vision (you can have multiple versions of S32DS installed on one machine)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Import S32V SDK example into the workspace by selecting menu File -&amp;gt; New -&amp;gt; S32DS Project from Example:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/75769iBEE1EB79D387F9E1/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_6.png" alt="pastedImage_6.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Note:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; The VSDK should be integrated into S32DS for S32 Platform at the beginning of Q2/2019&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Jan 2019 09:03:33 GMT</pubDate>
    <dc:creator>stanish</dc:creator>
    <dc:date>2019-01-23T09:03:33Z</dc:date>
    <item>
      <title>CAN interface Demo is needed</title>
      <link>https://community.nxp.com/t5/S32-SDK/CAN-interface-Demo-is-needed/m-p/854251#M767</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Recently , I am going to use M4 core existed in S32V234 platform to implement some applications , However ,I found no demos on CAN interface in S32DS For Vision, My specific platform is S32V234-EVB , I wonder if anyone could support me with this demo on CAN inetrface . any help would be needed , thank you .&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Jan 2019 08:06:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/CAN-interface-Demo-is-needed/m-p/854251#M767</guid>
      <dc:creator>frank_feng</dc:creator>
      <dc:date>2019-01-23T08:06:38Z</dc:date>
    </item>
    <item>
      <title>Re: CAN interface Demo is needed</title>
      <link>https://community.nxp.com/t5/S32-SDK/CAN-interface-Demo-is-needed/m-p/854252#M768</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually there is a FlexCAN example available. It's based on s32V234 SDK v0.8.1 (EAR) that is currently part of S32DS for S32 Platform only.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-342447"&gt;S32 Design Studio 2018.R1 for S32 Automotive ARM Platform (Windows/Linux) released!&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd recommend you to install this version + S32V2xx development package as described in the release announcement. It can coexist with S32DS for Vision (you can have multiple versions of S32DS installed on one machine)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Import S32V SDK example into the workspace by selecting menu File -&amp;gt; New -&amp;gt; S32DS Project from Example:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/75769iBEE1EB79D387F9E1/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_6.png" alt="pastedImage_6.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Note:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; The VSDK should be integrated into S32DS for S32 Platform at the beginning of Q2/2019&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Jan 2019 09:03:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/CAN-interface-Demo-is-needed/m-p/854252#M768</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2019-01-23T09:03:33Z</dc:date>
    </item>
  </channel>
</rss>