<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 SDK中的主题 Re: Question with clock transfer mode on MPC5744P</title>
    <link>https://community.nxp.com/t5/S32-SDK/Question-with-clock-transfer-mode-on-MPC5744P/m-p/845760#M720</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suspect there could be an issue related to a pending interrupt in the bootloader application.&lt;/P&gt;&lt;P&gt;Before you jump to your application from bootloader I'd suggest you to deinitialize drivers.&lt;/P&gt;&lt;P&gt;Since there is no reset before entering application from bootloader the the device is not in the default state.&amp;nbsp;&lt;/P&gt;&lt;P&gt;SDK offers de-initialization API for this purpose e.g. for PIT timer -&amp;nbsp;&amp;nbsp;&lt;EM&gt;&lt;STRONG&gt;PIT_DRV_Deinit(INST_PIT1);&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you possibly attach your zipped projects if it does not help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 Jan 2019 16:33:07 GMT</pubDate>
    <dc:creator>stanish</dc:creator>
    <dc:date>2019-01-04T16:33:07Z</dc:date>
    <item>
      <title>Question with clock transfer mode on MPC5744P</title>
      <link>https://community.nxp.com/t5/S32-SDK/Question-with-clock-transfer-mode-on-MPC5744P/m-p/845757#M717</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;First，I build two new projects。one jumps to other one。Then， I add spi mode and jump to other one。It is dead on clock transfer mode and mode transfer timeout which apps that i jumped。I also try to add fccu mode or freertos mode，anyone cases this problem!&lt;BR /&gt; I have never see this problem， anybody can tell why？thanks，i use SDK&amp;nbsp; RTM 1.0.0.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jan 2019 06:46:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Question-with-clock-transfer-mode-on-MPC5744P/m-p/845757#M717</guid>
      <dc:creator>1376843253</dc:creator>
      <dc:date>2019-01-02T06:46:17Z</dc:date>
    </item>
    <item>
      <title>Re: Question with clock transfer mode on MPC5744P</title>
      <link>https://community.nxp.com/t5/S32-SDK/Question-with-clock-transfer-mode-on-MPC5744P/m-p/845758#M718</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help me to clarify if I understand this issue correctly.&lt;/P&gt;&lt;P&gt;Could you possibly specify which board are you using? (DevKit / EVB / Custom board)&lt;/P&gt;&lt;P&gt;Does the problem occurs if you debug a single SDK project?&lt;/P&gt;&lt;P&gt;Can you try to create a new SDK project from example e.g. "pit_periodic_interrupt_mpc5744p"&lt;/P&gt;&lt;P&gt;generate the code, build and debug. Are you able to pass mode transition in this project?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now if you are jumping from one project to the other - does it mean you have a bootloader and application?&lt;/P&gt;&lt;P&gt;So the bootloader project pass the clock init whereas the application which you jump into does not pass the clock initialization?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This will help us to resolve this issue much faster.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Jan 2019 15:48:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Question-with-clock-transfer-mode-on-MPC5744P/m-p/845758#M718</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2019-01-03T15:48:52Z</dc:date>
    </item>
    <item>
      <title>Re: Question with clock transfer mode on MPC5744P</title>
      <link>https://community.nxp.com/t5/S32-SDK/Question-with-clock-transfer-mode-on-MPC5744P/m-p/845759#M719</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I&amp;nbsp;used DEVKIT board.&lt;/P&gt;&lt;P&gt;I debug two projects(bootloader and app) by IC5000.&lt;/P&gt;&lt;P&gt;Yes,I tried.&amp;nbsp; In single project ,the clock mode transfer can be completed.&lt;/P&gt;&lt;P&gt;But,when&amp;nbsp;I jump to app,It is dead. The clock mode transfer like DRUN to DRUN is failed.&lt;/P&gt;&lt;P&gt;Yeah,I have a&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;bootloader and application. T&lt;SPAN&gt;he bootloader project pass the clock init,The app clock mode transfer (DRUN to DRUN) is failed.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/71439i5369EC823750BE4E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&amp;nbsp; &amp;nbsp; The bit S_MTRANS can not&amp;nbsp;become&amp;nbsp;to&amp;nbsp;0.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;&amp;nbsp;whatever,thanks!!!&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jan 2019 09:23:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Question-with-clock-transfer-mode-on-MPC5744P/m-p/845759#M719</guid>
      <dc:creator>1376843253</dc:creator>
      <dc:date>2019-01-04T09:23:46Z</dc:date>
    </item>
    <item>
      <title>Re: Question with clock transfer mode on MPC5744P</title>
      <link>https://community.nxp.com/t5/S32-SDK/Question-with-clock-transfer-mode-on-MPC5744P/m-p/845760#M720</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suspect there could be an issue related to a pending interrupt in the bootloader application.&lt;/P&gt;&lt;P&gt;Before you jump to your application from bootloader I'd suggest you to deinitialize drivers.&lt;/P&gt;&lt;P&gt;Since there is no reset before entering application from bootloader the the device is not in the default state.&amp;nbsp;&lt;/P&gt;&lt;P&gt;SDK offers de-initialization API for this purpose e.g. for PIT timer -&amp;nbsp;&amp;nbsp;&lt;EM&gt;&lt;STRONG&gt;PIT_DRV_Deinit(INST_PIT1);&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you possibly attach your zipped projects if it does not help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jan 2019 16:33:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Question-with-clock-transfer-mode-on-MPC5744P/m-p/845760#M720</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2019-01-04T16:33:07Z</dc:date>
    </item>
  </channel>
</rss>