<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ENET on DEVKIT MPC5748G in S32 SDK</title>
    <link>https://community.nxp.com/t5/S32-SDK/ENET-on-DEVKIT-MPC5748G/m-p/682250#M61</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Was able to figure out the pin_mux issue out. After that the compile went on fine.&lt;/P&gt;&lt;P&gt;Yes, after adding the arp entry it pings just fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Tiju&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Jul 2017 16:13:49 GMT</pubDate>
    <dc:creator>tiju</dc:creator>
    <dc:date>2017-07-27T16:13:49Z</dc:date>
    <item>
      <title>ENET on DEVKIT MPC5748G</title>
      <link>https://community.nxp.com/t5/S32-SDK/ENET-on-DEVKIT-MPC5748G/m-p/682248#M59</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I try to build the processor expert code from the example - enet_ping_mpc5748g, I get the following error. Do we need to do some other config for this to work?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/26938i7CBADE985F418014/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/26980i9CF694B9749DD201/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone help to resolve the issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Tiju&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jul 2017 05:03:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/ENET-on-DEVKIT-MPC5748G/m-p/682248#M59</guid>
      <dc:creator>tiju</dc:creator>
      <dc:date>2017-07-26T05:03:38Z</dc:date>
    </item>
    <item>
      <title>Re: ENET on DEVKIT MPC5748G</title>
      <link>https://community.nxp.com/t5/S32-SDK/ENET-on-DEVKIT-MPC5748G/m-p/682249#M60</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Tiju,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the report.&lt;/P&gt;&lt;P&gt;I noticed that the pin_mux component is missing a pin direction setup.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/29459i9A4A9EC47D5F2A78/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please adjust &amp;nbsp;ENET0 RMII Transmit Clock pin as output and regenerate code:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/29553i850D72CDB1DE44C1/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now you should be able to build and debug the project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding the C errors in Problem View -&amp;gt; this is a known eclipse issue, please try the workaround described here:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/message/924323#comment-924619" title="https://community.nxp.com/message/924323#comment-924619"&gt;https://community.nxp.com/message/924323#comment-924619&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: Before pinging the DevKit don't forget to update the ARP table on your PC manually. This example does not process ARP request packets.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jul 2017 15:09:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/ENET-on-DEVKIT-MPC5748G/m-p/682249#M60</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2017-07-26T15:09:52Z</dc:date>
    </item>
    <item>
      <title>Re: ENET on DEVKIT MPC5748G</title>
      <link>https://community.nxp.com/t5/S32-SDK/ENET-on-DEVKIT-MPC5748G/m-p/682250#M61</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Was able to figure out the pin_mux issue out. After that the compile went on fine.&lt;/P&gt;&lt;P&gt;Yes, after adding the arp entry it pings just fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Tiju&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jul 2017 16:13:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/ENET-on-DEVKIT-MPC5748G/m-p/682250#M61</guid>
      <dc:creator>tiju</dc:creator>
      <dc:date>2017-07-27T16:13:49Z</dc:date>
    </item>
  </channel>
</rss>