<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 SDKのトピックS32K</title>
    <link>https://community.nxp.com/t5/S32-SDK/S32K/m-p/813583#M578</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How can I use the SDK realise next function:&lt;/P&gt;&lt;P&gt;the MCU is the master device, I want to use flexio or LPI2C read/write slave device subaddress(such as EEPROM , own&amp;nbsp; subaddress). I lookup the SDK interface, dont get the subaddress access operation.&lt;/P&gt;&lt;P&gt;How CAN I do it use the SDK?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Oct 2018 03:30:50 GMT</pubDate>
    <dc:creator>weill</dc:creator>
    <dc:date>2018-10-22T03:30:50Z</dc:date>
    <item>
      <title>S32K</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K/m-p/813583#M578</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How can I use the SDK realise next function:&lt;/P&gt;&lt;P&gt;the MCU is the master device, I want to use flexio or LPI2C read/write slave device subaddress(such as EEPROM , own&amp;nbsp; subaddress). I lookup the SDK interface, dont get the subaddress access operation.&lt;/P&gt;&lt;P&gt;How CAN I do it use the SDK?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Oct 2018 03:30:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K/m-p/813583#M578</guid>
      <dc:creator>weill</dc:creator>
      <dc:date>2018-10-22T03:30:50Z</dc:date>
    </item>
    <item>
      <title>Re: S32K</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K/m-p/813584#M579</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You need to use the SDK functions, such as&amp;nbsp;LPI2C_DRV_MasterSendDataBlocking(), to send a sub-address or a command to the slave, you also need to specify if the function will send Stop condition&amp;nbsp;- the function takes that&amp;nbsp;as an argument.&amp;nbsp;The SDK PE interface allows you to select the address of the slave device only.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Oct 2018 14:56:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K/m-p/813584#M579</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-10-25T14:56:00Z</dc:date>
    </item>
  </channel>
</rss>