<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic fatal error: device_registers.h: No such file or directory in S32 SDK</title>
    <link>https://community.nxp.com/t5/S32-SDK/fatal-error-device-registers-h-No-such-file-or-directory/m-p/773758#M418</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The total error message is:&lt;/P&gt;&lt;P&gt;../Generated_Code/Cpu.h:61:30: fatal error: device_registers.h: No such file or directory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using S32 Design Studio for Power Architecture and create&amp;nbsp;&amp;nbsp;a example project named pit_periodic_interrupt through menuitem "S32DS Project from example".But by default,the project have only two configuration options:Debug_Flash &amp;amp; Debug_RAM,i wanna create a release version bin file,so i create a new configuration option named "Release" in "Create New Configuration" dialog,and i choose the "Default configuration" option and&amp;nbsp;select the "Rlease" in dropdown list.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then first i generate the PE codes,after that i build the project and get the error message.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I find the device_registers.h in&amp;nbsp;${S32_SDK_PATH}/platform/devices,so i add this path into "Standard S32DS C Compiler".Includes,but still doesn't work.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 26 Feb 2018 02:19:30 GMT</pubDate>
    <dc:creator>everkimage</dc:creator>
    <dc:date>2018-02-26T02:19:30Z</dc:date>
    <item>
      <title>fatal error: device_registers.h: No such file or directory</title>
      <link>https://community.nxp.com/t5/S32-SDK/fatal-error-device-registers-h-No-such-file-or-directory/m-p/773758#M418</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The total error message is:&lt;/P&gt;&lt;P&gt;../Generated_Code/Cpu.h:61:30: fatal error: device_registers.h: No such file or directory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using S32 Design Studio for Power Architecture and create&amp;nbsp;&amp;nbsp;a example project named pit_periodic_interrupt through menuitem "S32DS Project from example".But by default,the project have only two configuration options:Debug_Flash &amp;amp; Debug_RAM,i wanna create a release version bin file,so i create a new configuration option named "Release" in "Create New Configuration" dialog,and i choose the "Default configuration" option and&amp;nbsp;select the "Rlease" in dropdown list.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then first i generate the PE codes,after that i build the project and get the error message.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I find the device_registers.h in&amp;nbsp;${S32_SDK_PATH}/platform/devices,so i add this path into "Standard S32DS C Compiler".Includes,but still doesn't work.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Feb 2018 02:19:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/fatal-error-device-registers-h-No-such-file-or-directory/m-p/773758#M418</guid>
      <dc:creator>everkimage</dc:creator>
      <dc:date>2018-02-26T02:19:30Z</dc:date>
    </item>
    <item>
      <title>Re: fatal error: device_registers.h: No such file or directory</title>
      <link>https://community.nxp.com/t5/S32-SDK/fatal-error-device-registers-h-No-such-file-or-directory/m-p/773759#M419</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the example projects are little bit different than standard ones (they used linked files and so on) and it is hard and time consuming to configure another build target.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you need release version - you can remove debug option from gcc parameters for Flash target - right click on project name -&amp;gt; properties -&amp;gt; C/C++ build -&amp;gt; Settings&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/19065iC4076B5B72A3AFA9/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Feb 2018 07:40:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/fatal-error-device-registers-h-No-such-file-or-directory/m-p/773759#M419</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2018-02-26T07:40:59Z</dc:date>
    </item>
    <item>
      <title>Re: fatal error: device_registers.h: No such file or directory</title>
      <link>https://community.nxp.com/t5/S32-SDK/fatal-error-device-registers-h-No-such-file-or-directory/m-p/773760#M420</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It's ok to create a new configuration by copy from default configurations and then remove the debug option.&lt;/P&gt;&lt;P&gt;Thanks for you answer.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Feb 2018 09:39:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/fatal-error-device-registers-h-No-such-file-or-directory/m-p/773760#M420</guid>
      <dc:creator>everkimage</dc:creator>
      <dc:date>2018-02-26T09:39:51Z</dc:date>
    </item>
  </channel>
</rss>