<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Request for Assistance with SPI Communication in NXP Libraries in S32 SDK</title>
    <link>https://community.nxp.com/t5/S32-SDK/Request-for-Assistance-with-SPI-Communication-in-NXP-Libraries/m-p/2109779#M4059</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229702"&gt;@Anilpatil_SasvaAuto&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;I suggest using the example inside the RTD package, as there are no newer examples posted in community for now.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_0-1748982314404.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/341185iCC1E62DABA6EB781/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Julin_AragnM_0-1748982314404.png" alt="Julin_AragnM_0-1748982314404.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Julin_AragnM_0-1748982314404.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Still, you can refer to some old posts, such as:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-LPIT-DMA-LPSPI/ta-p/1108628" target="_blank"&gt;Example S32K144 LPIT DMA LPSPI - NXP Community&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
    <pubDate>Tue, 03 Jun 2025 20:25:37 GMT</pubDate>
    <dc:creator>Julián_AragónM</dc:creator>
    <dc:date>2025-06-03T20:25:37Z</dc:date>
    <item>
      <title>Request for Assistance with SPI Communication in NXP Libraries</title>
      <link>https://community.nxp.com/t5/S32-SDK/Request-for-Assistance-with-SPI-Communication-in-NXP-Libraries/m-p/2107786#M4056</link>
      <description>&lt;P&gt;Hello Team,&lt;/P&gt;&lt;P&gt;I am currently using the NXP SE Host library for the NCJ37A secure element in my project. I have noticed that the library employs a blocking method for SPI communication. I would like to request an example of an SPI driver that utilizes interrupts instead.&lt;/P&gt;&lt;P&gt;Additionally, I have integrated the "aNfcRdLib_SDK_Evaluation_v2.28" NFC reader library within the same project. Could you clarify whether this NFC reader library uses a blocking or non-blocking approach for SPI communication? If it employs a blocking method, I would appreciate guidance on how to implement a non-blocking SPI driver.&lt;/P&gt;&lt;P&gt;After integrating both example libraries provided by NXP, I observed that the applications execute independently without interfering with each other. However, when I try to run both applications simultaneously, only one works—the SE NCJ37A is functional, while the NFC reader is not.&lt;/P&gt;&lt;P&gt;Both clock configurations are different, SPI clock is also different.&lt;/P&gt;&lt;P&gt;Thank you for your assistance.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 30 May 2025 07:33:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Request-for-Assistance-with-SPI-Communication-in-NXP-Libraries/m-p/2107786#M4056</guid>
      <dc:creator>Anilpatil_SasvaAuto</dc:creator>
      <dc:date>2025-05-30T07:33:30Z</dc:date>
    </item>
    <item>
      <title>Re: Request for Assistance with SPI Communication in NXP Libraries</title>
      <link>https://community.nxp.com/t5/S32-SDK/Request-for-Assistance-with-SPI-Communication-in-NXP-Libraries/m-p/2108137#M4057</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229702"&gt;@Anilpatil_SasvaAuto&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;There is actually an example for SPI communication using interrupts, please refer to this community post:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-SPI-Transmit-amp-Receive-Using-Interrupt-DS3-5/ta-p/2011866" target="_blank"&gt;Example S32K312 SPI Transmit &amp;amp; Receive Using Interrupt DS3.5 RTD300 - NXP Community.&lt;/A&gt;&amp;nbsp;Or, if you are using S32K1, the RTD package already includes examples for SPI interrupt, such as the&amp;nbsp;&lt;STRONG&gt;Lpspi_Ip_HalfDuplex_Transfer_S32K1XX&amp;nbsp;&lt;/STRONG&gt;example.&lt;/P&gt;
&lt;P&gt;However, if you need assistance with the aNFC library, please contact the respective team directly (at:&amp;nbsp;&lt;A href="mailto:automotive_nfc@nxp.com" target="_blank"&gt;automotive_nfc@nxp.com&lt;/A&gt;).&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 30 May 2025 15:53:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Request-for-Assistance-with-SPI-Communication-in-NXP-Libraries/m-p/2108137#M4057</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2025-05-30T15:53:53Z</dc:date>
    </item>
    <item>
      <title>Re: Request for Assistance with SPI Communication in NXP Libraries</title>
      <link>https://community.nxp.com/t5/S32-SDK/Request-for-Assistance-with-SPI-Communication-in-NXP-Libraries/m-p/2108465#M4058</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello Julián,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The example code in the provided link is for the S32K3XX micro, but I need it for the S32K144. could you please provide the same?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 02 Jun 2025 07:07:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Request-for-Assistance-with-SPI-Communication-in-NXP-Libraries/m-p/2108465#M4058</guid>
      <dc:creator>Anilpatil_SasvaAuto</dc:creator>
      <dc:date>2025-06-02T07:07:31Z</dc:date>
    </item>
    <item>
      <title>Re: Request for Assistance with SPI Communication in NXP Libraries</title>
      <link>https://community.nxp.com/t5/S32-SDK/Request-for-Assistance-with-SPI-Communication-in-NXP-Libraries/m-p/2109779#M4059</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229702"&gt;@Anilpatil_SasvaAuto&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;I suggest using the example inside the RTD package, as there are no newer examples posted in community for now.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_0-1748982314404.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/341185iCC1E62DABA6EB781/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Julin_AragnM_0-1748982314404.png" alt="Julin_AragnM_0-1748982314404.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Julin_AragnM_0-1748982314404.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Still, you can refer to some old posts, such as:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-LPIT-DMA-LPSPI/ta-p/1108628" target="_blank"&gt;Example S32K144 LPIT DMA LPSPI - NXP Community&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Tue, 03 Jun 2025 20:25:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Request-for-Assistance-with-SPI-Communication-in-NXP-Libraries/m-p/2109779#M4059</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2025-06-03T20:25:37Z</dc:date>
    </item>
  </channel>
</rss>