<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 SDKのトピックS32 fails to set System OSC?</title>
    <link>https://community.nxp.com/t5/S32-SDK/S32-fails-to-set-System-OSC/m-p/548790#M4</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;I'm working with an S32 dev board, and trying to get some code working to send CAN messages on a periodic basis. When I run into issues working with a component (CAN SBC in this case) I'll occasionally set up a S32DS project based off of one of the examples during Vlad's class at FTF to try and isolate the problem. This time, however, I followed the directions step by step from the example but the program keeps getting caught in the Watchdog IRQ.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've noticed this can often happen if a peripheral doesn't have a clock gated to it or something, but I've double checked everything I can think of but it seems to get stuck on CLOCK_SYS_INIT(); - -I've attached the project here, does anyone have any idea what I might've screwed up/ what to check?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Jul 2016 23:07:49 GMT</pubDate>
    <dc:creator>gearhead1107</dc:creator>
    <dc:date>2016-07-28T23:07:49Z</dc:date>
    <item>
      <title>S32 fails to set System OSC?</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32-fails-to-set-System-OSC/m-p/548790#M4</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;I'm working with an S32 dev board, and trying to get some code working to send CAN messages on a periodic basis. When I run into issues working with a component (CAN SBC in this case) I'll occasionally set up a S32DS project based off of one of the examples during Vlad's class at FTF to try and isolate the problem. This time, however, I followed the directions step by step from the example but the program keeps getting caught in the Watchdog IRQ.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've noticed this can often happen if a peripheral doesn't have a clock gated to it or something, but I've double checked everything I can think of but it seems to get stuck on CLOCK_SYS_INIT(); - -I've attached the project here, does anyone have any idea what I might've screwed up/ what to check?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jul 2016 23:07:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32-fails-to-set-System-OSC/m-p/548790#M4</guid>
      <dc:creator>gearhead1107</dc:creator>
      <dc:date>2016-07-28T23:07:49Z</dc:date>
    </item>
    <item>
      <title>Re: S32 fails to set System OSC?</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32-fails-to-set-System-OSC/m-p/548791#M5</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I checked the project and I cannot reproduce the issue you described. Can you possibly post the step-by-step instruction &amp;nbsp;how to get to WDG IRQ handler? do I need to generate a traffic on CAN bus?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Aug 2016 15:13:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32-fails-to-set-System-OSC/m-p/548791#M5</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2016-08-29T15:13:22Z</dc:date>
    </item>
    <item>
      <title>Re: S32 fails to set System OSC?</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32-fails-to-set-System-OSC/m-p/548792#M6</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey Stan, don't sweat it - I started a new project and the code ran fine - must've been an eclipse issue&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Aug 2016 15:16:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32-fails-to-set-System-OSC/m-p/548792#M6</guid>
      <dc:creator>gearhead1107</dc:creator>
      <dc:date>2016-08-29T15:16:48Z</dc:date>
    </item>
  </channel>
</rss>