<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 SDKのトピックRe: S32K Lpuart Rx overrun error</title>
    <link>https://community.nxp.com/t5/S32-SDK/S32K-Lpuart-Rx-overrun-error/m-p/1909586#M3901</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200831"&gt;@Julián_AragónM&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your response.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tested one byte and it is working fine.&amp;nbsp;&lt;/P&gt;&lt;P&gt;When the request is on a continuous mode, it is throwing OR error after sometime.&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
    <pubDate>Tue, 16 Jul 2024 08:55:23 GMT</pubDate>
    <dc:creator>Dev15</dc:creator>
    <dc:date>2024-07-16T08:55:23Z</dc:date>
    <item>
      <title>S32K Lpuart Rx overrun error</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K-Lpuart-Rx-overrun-error/m-p/1908453#M3895</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have configured LPUART 1 interrupt mode and facing receive over run error. Below are the some details on the version and configurations&lt;/P&gt;&lt;P&gt;S32 Design Studio for S32 Platform&lt;BR /&gt;Version: 3.5&lt;/P&gt;&lt;P&gt;RTD: 3.0.0&lt;/P&gt;&lt;P&gt;Baud rate set : 9600&lt;/P&gt;&lt;P&gt;I'm trying to read with in the callback configured.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Dev15_0-1721028789540.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/288512i6739C6165DEE2D73/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Dev15_0-1721028789540.png" alt="Dev15_0-1721028789540.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Dev15_0-1721028789540.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please help on this issue,&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 15 Jul 2024 07:35:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K-Lpuart-Rx-overrun-error/m-p/1908453#M3895</guid>
      <dc:creator>Dev15</dc:creator>
      <dc:date>2024-07-15T07:35:58Z</dc:date>
    </item>
    <item>
      <title>Re: S32K Lpuart Rx overrun error</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K-Lpuart-Rx-overrun-error/m-p/1909030#M3900</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/227246"&gt;@Dev15&lt;/a&gt;,&lt;/P&gt;
&lt;P lang="es-MX"&gt;Normally this issue is caused by priority configuration. It could be solved by increasing the system clock frequency or decreasing the BaudRate.&lt;/P&gt;
&lt;P lang="es-MX"&gt;Are you testing the reception with the CAN echo? Could you transfer just one byte at a time to test reception? This community post solved an overrun issue by moving the&amp;nbsp;&lt;SPAN&gt;SendData function into the rxCallback function:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/uart-pal-s32k144w-status-STATUS-UART-RX-OVERRUN/m-p/1425502" target="_blank"&gt;uart_pal_s32k144w status = STATUS_UART_RX_OVERRUN - NXP Community&lt;/A&gt;.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P lang="es-MX"&gt;&lt;SPAN&gt;Since you are using RTD 3.0.0, I assume you are using S32K3. You can look into this community post as reference as well:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/The-S32K344-Lpuart-transfer-cannot-receive-data-correctly-when/m-p/1856599" target="_blank"&gt;Solved: The S32K344 Lpuart transfer cannot receive data correctly when DMA enable - NXP Community&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P lang="es-MX"&gt;&lt;SPAN&gt;Best regards;&lt;BR /&gt;Julián&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 15 Jul 2024 18:31:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K-Lpuart-Rx-overrun-error/m-p/1909030#M3900</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-07-15T18:31:25Z</dc:date>
    </item>
    <item>
      <title>Re: S32K Lpuart Rx overrun error</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K-Lpuart-Rx-overrun-error/m-p/1909586#M3901</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200831"&gt;@Julián_AragónM&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your response.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tested one byte and it is working fine.&amp;nbsp;&lt;/P&gt;&lt;P&gt;When the request is on a continuous mode, it is throwing OR error after sometime.&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Tue, 16 Jul 2024 08:55:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K-Lpuart-Rx-overrun-error/m-p/1909586#M3901</guid>
      <dc:creator>Dev15</dc:creator>
      <dc:date>2024-07-16T08:55:23Z</dc:date>
    </item>
  </channel>
</rss>