<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 SDKのトピックRe: EEP Partitioning causing exception or Hardfault during Init after flashing</title>
    <link>https://community.nxp.com/t5/S32-SDK/EEP-Partitioning-causing-exception-or-Hardfault-during-Init/m-p/1892704#M3857</link>
    <description>&lt;P&gt;How do you force the function to RAM?&lt;/P&gt;</description>
    <pubDate>Mon, 24 Jun 2024 08:04:09 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2024-06-24T08:04:09Z</dc:date>
    <item>
      <title>EEP Partitioning causing exception or Hardfault during Init after flashing</title>
      <link>https://community.nxp.com/t5/S32-SDK/EEP-Partitioning-causing-exception-or-Hardfault-during-Init/m-p/1881449#M3788</link>
      <description>&lt;P&gt;I have developed a custom SW for&amp;nbsp;S32K118, in which I have to store Data to NVM, for this I have used FlexRAM.&amp;nbsp;&lt;SPAN&gt;When I flashed App on the MCU and run, I observe that MCU stuck at exception handler. After debugging the SW I have seen that, while FlexRAM partition is in progress its going to exception&amp;nbsp; from the condition "while(0 == ((FTFC-&amp;gt;FSTAT &amp;amp; FTFC_FSTAT_CCIF_MASK) &amp;gt;&amp;gt; FTFC_FSTAT_CCIF_SHIFT))" is being checked, &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Note: also the watchdog is enabled before the partitioning with timeout of 32mSec and refresh is performed every 10mSec. The FlexRAM activity is performed in periodic task of 10mSec for partitioning/Reading/Writing. Also MCU reset is performed after EEP partition as per the requirement.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jun 2024 10:30:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/EEP-Partitioning-causing-exception-or-Hardfault-during-Init/m-p/1881449#M3788</guid>
      <dc:creator>SAnjal</dc:creator>
      <dc:date>2024-06-05T10:30:42Z</dc:date>
    </item>
    <item>
      <title>Re: EEP Partitioning causing exception or Hardfault during Init after flashing</title>
      <link>https://community.nxp.com/t5/S32-SDK/EEP-Partitioning-causing-exception-or-Hardfault-during-Init/m-p/1883712#M3795</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/216404"&gt;@SAnjal&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The partition command must be executed from RAM memory. You need to ensure that the flash is not accessed during partitioning (disabled interrupts, callback function in RAM...):&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lukaszadrapa_0-1717775002465.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/283103i16C37981EBA05D0C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="lukaszadrapa_0-1717775002465.png" alt="lukaszadrapa_0-1717775002465.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;And be aware of other restrictions related to flash, emulated eeprom and CSEc:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lukaszadrapa_1-1717775067559.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/283104iBA539B101E04E2D2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="lukaszadrapa_1-1717775067559.png" alt="lukaszadrapa_1-1717775067559.png" /&gt;&lt;/span&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 07 Jun 2024 15:45:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/EEP-Partitioning-causing-exception-or-Hardfault-during-Init/m-p/1883712#M3795</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2024-06-07T15:45:28Z</dc:date>
    </item>
    <item>
      <title>Re: EEP Partitioning causing exception or Hardfault during Init after flashing</title>
      <link>https://community.nxp.com/t5/S32-SDK/EEP-Partitioning-causing-exception-or-Hardfault-during-Init/m-p/1890310#M3837</link>
      <description>&lt;P&gt;We have take care to run Partitioning command from RAM but, still facing this issue. As per observation,&lt;/P&gt;&lt;P&gt;PC is not jumping to RAM to execute the Program Partitioning command.&lt;/P&gt;&lt;P&gt;Note: As per current implementation we have optimized our code to level 01, does this might be creating the issue. If yes, then what care should we take for FlexRAM partitioning.&lt;/P&gt;</description>
      <pubDate>Wed, 19 Jun 2024 10:34:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/EEP-Partitioning-causing-exception-or-Hardfault-during-Init/m-p/1890310#M3837</guid>
      <dc:creator>SAnjal</dc:creator>
      <dc:date>2024-06-19T10:34:58Z</dc:date>
    </item>
    <item>
      <title>Re: EEP Partitioning causing exception or Hardfault during Init after flashing</title>
      <link>https://community.nxp.com/t5/S32-SDK/EEP-Partitioning-causing-exception-or-Hardfault-during-Init/m-p/1892704#M3857</link>
      <description>&lt;P&gt;How do you force the function to RAM?&lt;/P&gt;</description>
      <pubDate>Mon, 24 Jun 2024 08:04:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/EEP-Partitioning-causing-exception-or-Hardfault-during-Init/m-p/1892704#M3857</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2024-06-24T08:04:09Z</dc:date>
    </item>
  </channel>
</rss>