<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32 DS for ARM compile error. in S32 SDK</title>
    <link>https://community.nxp.com/t5/S32-SDK/S32-DS-for-ARM-compile-error/m-p/757280#M374</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;To test the S32144 EVB, Through S32DS, I generated code. &lt;BR /&gt;I used pwm_pal1 components&amp;nbsp; and compile the code.&lt;BR /&gt;But following error is occured.&lt;BR /&gt;"SDK/platform/pal/pwm/inc/pwm_pal.h:150:28: error: unknown type name 'pwm_instance_t'"&lt;BR /&gt;It is the reason that CPU_S32K144HFT0VLLT or CPU_S32K144LFT0MLLT is not defined.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to resolve this error?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 Jun 2018 05:11:33 GMT</pubDate>
    <dc:creator>kbj</dc:creator>
    <dc:date>2018-06-07T05:11:33Z</dc:date>
    <item>
      <title>S32 DS for ARM compile error.</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32-DS-for-ARM-compile-error/m-p/757280#M374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;To test the S32144 EVB, Through S32DS, I generated code. &lt;BR /&gt;I used pwm_pal1 components&amp;nbsp; and compile the code.&lt;BR /&gt;But following error is occured.&lt;BR /&gt;"SDK/platform/pal/pwm/inc/pwm_pal.h:150:28: error: unknown type name 'pwm_instance_t'"&lt;BR /&gt;It is the reason that CPU_S32K144HFT0VLLT or CPU_S32K144LFT0MLLT is not defined.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to resolve this error?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jun 2018 05:11:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32-DS-for-ARM-compile-error/m-p/757280#M374</guid>
      <dc:creator>kbj</dc:creator>
      <dc:date>2018-06-07T05:11:33Z</dc:date>
    </item>
    <item>
      <title>Re: S32 DS for ARM compile error.</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32-DS-for-ARM-compile-error/m-p/757281#M375</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can you please share your project? Thanks.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jun 2018 06:53:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32-DS-for-ARM-compile-error/m-p/757281#M375</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2018-06-07T06:53:29Z</dc:date>
    </item>
    <item>
      <title>Re: S32 DS for ARM compile error.</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32-DS-for-ARM-compile-error/m-p/757282#M376</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;No projects are currently in progress.&lt;BR /&gt;I plan to use S32K144 in future projects, so I purchased the S32K144 EVB board and will implement the functions using S32 Design Studio.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Byungju.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jun 2018 07:27:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32-DS-for-ARM-compile-error/m-p/757282#M376</guid>
      <dc:creator>kbj</dc:creator>
      <dc:date>2018-06-07T07:27:47Z</dc:date>
    </item>
    <item>
      <title>Re: S32 DS for ARM compile error.</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32-DS-for-ARM-compile-error/m-p/757283#M377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;unfortunately - I can't reproduce your issue. Did you include&lt;/P&gt;&lt;P&gt;#include "pwm_pal1.h"&lt;BR /&gt;#include "pwm_pal_mapping.h"&lt;/P&gt;&lt;P&gt;Headers? the&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;pwm_instance_t is defined in pwm_pal_mapping.h - including the instance enums.&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Jiri&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jun 2018 08:26:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32-DS-for-ARM-compile-error/m-p/757283#M377</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2018-06-07T08:26:08Z</dc:date>
    </item>
    <item>
      <title>Re: S32 DS for ARM compile error.</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32-DS-for-ARM-compile-error/m-p/757284#M378</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Jiri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;DIV&gt;To reproduce, The spi component and the pwm component should be added and then recompiled.&lt;/DIV&gt;&lt;DIV&gt;As a result of my checking, adding pwm or spi component alone does not reproduce it.&lt;BR /&gt;It is also strange that the api of the pwm_pal component is the same as the api of the spi component.&lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;Refer to "3.PNG"&lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;Best regards,&lt;/DIV&gt;&lt;DIV&gt;Byungju.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jun 2018 08:58:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32-DS-for-ARM-compile-error/m-p/757284#M378</guid>
      <dc:creator>kbj</dc:creator>
      <dc:date>2018-06-07T08:58:55Z</dc:date>
    </item>
    <item>
      <title>Re: S32 DS for ARM compile error.</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32-DS-for-ARM-compile-error/m-p/757285#M379</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;finally I got it - thanks for report. There are two very same header defines for spi_pal and pwm_pal and -&amp;nbsp;#define PAL_mapping_H&amp;nbsp;&lt;/P&gt;&lt;P&gt;When PAL_mapping_H is defined by pwm_pal - spi_pal_mapping is disabled and vice versa. I'll create ticket for SDK team.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SPI functions in pwm_pal is known issue. It is fixed in&amp;nbsp;S32SDK_S32K14x_BETA_1.9.0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As workaround change In spi_pal_mapping.h file&amp;nbsp; PAL_mapping_H define to:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#ifndef SPI_PAL_mapping_H&lt;BR /&gt;#define SPI_PAL_mapping_H&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Don't forget that by re-generating PE code will be the change rewritten by Processor Expert. The #define issue is also fixed in&amp;nbsp;&lt;SPAN&gt;S32SDK_S32K14x_BETA_1.9.0&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jun 2018 10:30:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32-DS-for-ARM-compile-error/m-p/757285#M379</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2018-06-07T10:30:15Z</dc:date>
    </item>
    <item>
      <title>Re: S32 DS for ARM compile error.</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32-DS-for-ARM-compile-error/m-p/757286#M380</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks to that, I am able to solve the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Byungju.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jun 2018 23:30:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32-DS-for-ARM-compile-error/m-p/757286#M380</guid>
      <dc:creator>kbj</dc:creator>
      <dc:date>2018-06-07T23:30:32Z</dc:date>
    </item>
  </channel>
</rss>