<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 SDK中的主题 Re: Need LPUART2 using DMA example.</title>
    <link>https://community.nxp.com/t5/S32-SDK/Need-LPUART2-using-DMA-example/m-p/1836423#M3694</link>
    <description>&lt;P&gt;Hi Robin,&lt;/P&gt;&lt;P&gt;thanks for advice. I can compile now project and configuration looks correct, but nothing appears as input or output data. may you please take a look to the project attached to this post?&lt;/P&gt;</description>
    <pubDate>Wed, 27 Mar 2024 14:26:33 GMT</pubDate>
    <dc:creator>paulffffff</dc:creator>
    <dc:date>2024-03-27T14:26:33Z</dc:date>
    <item>
      <title>Need LPUART2 using DMA example.</title>
      <link>https://community.nxp.com/t5/S32-SDK/Need-LPUART2-using-DMA-example/m-p/1834874#M3683</link>
      <description>&lt;P&gt;I used provided example for LPUART0 using DMA for MR-CANHUBS32K344 board:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K/S32K3-LPUART-using-DMA-in-RTD-3-0-0/m-p/1737356?_gl=1*1gwjclh*_ga*MTA3NTA1NDUzMy4xNzA5OTE3OTQ3*_ga_WM5LE0KMSH*MTcxMTA4MzM3Mi43LjEuMTcxMTA4Mzk3Ny4wLjAuMA.." target="_blank" rel="noopener"&gt;Solved: S32K3 LPUART using DMA in RTD 3.0.0 - NXP Community&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;But I cannot configure tis example to use with LPUART2, which is routed and connected to debug connector and can be easy accessed. May you provide modified example for LPUART2 using DMA vs LPUART0 using DMA?&lt;/P&gt;</description>
      <pubDate>Mon, 25 Mar 2024 20:34:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Need-LPUART2-using-DMA-example/m-p/1834874#M3683</guid>
      <dc:creator>paulffffff</dc:creator>
      <dc:date>2024-03-25T20:34:55Z</dc:date>
    </item>
    <item>
      <title>Re: Need LPUART2 using DMA example.</title>
      <link>https://community.nxp.com/t5/S32-SDK/Need-LPUART2-using-DMA-example/m-p/1836163#M3692</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Did you change the configuration of&amp;nbsp;LPUART2 in Rm &lt;STRONG&gt;Dma Mux&lt;/STRONG&gt;?&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="LPUART2 Rm Dma Mux.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/270651i04F0947B642BC77B/image-size/large?v=v2&amp;amp;px=999" role="button" title="LPUART2 Rm Dma Mux.png" alt="LPUART2 Rm Dma Mux.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Mar 2024 08:38:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Need-LPUART2-using-DMA-example/m-p/1836163#M3692</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-03-27T08:38:19Z</dc:date>
    </item>
    <item>
      <title>Re: Need LPUART2 using DMA example.</title>
      <link>https://community.nxp.com/t5/S32-SDK/Need-LPUART2-using-DMA-example/m-p/1836423#M3694</link>
      <description>&lt;P&gt;Hi Robin,&lt;/P&gt;&lt;P&gt;thanks for advice. I can compile now project and configuration looks correct, but nothing appears as input or output data. may you please take a look to the project attached to this post?&lt;/P&gt;</description>
      <pubDate>Wed, 27 Mar 2024 14:26:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Need-LPUART2-using-DMA-example/m-p/1836423#M3694</guid>
      <dc:creator>paulffffff</dc:creator>
      <dc:date>2024-03-27T14:26:33Z</dc:date>
    </item>
    <item>
      <title>Re: Need LPUART2 using DMA example.</title>
      <link>https://community.nxp.com/t5/S32-SDK/Need-LPUART2-using-DMA-example/m-p/1839298#M3703</link>
      <description>&lt;P&gt;Seems that you forget change the&amp;nbsp;&lt;STRONG&gt;Hardware Channel&lt;/STRONG&gt; in&amp;nbsp;&lt;STRONG&gt;Dma Logic Channel&lt;/STRONG&gt;:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Dma Logic Channel Hardware Channel.png" style="width: 942px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/271546i41DFD961371FC7A4/image-size/large?v=v2&amp;amp;px=999" role="button" title="Dma Logic Channel Hardware Channel.png" alt="Dma Logic Channel Hardware Channel.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Apr 2024 11:13:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Need-LPUART2-using-DMA-example/m-p/1839298#M3703</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-04-02T11:13:28Z</dc:date>
    </item>
    <item>
      <title>Re: Need LPUART2 using DMA example.</title>
      <link>https://community.nxp.com/t5/S32-SDK/Need-LPUART2-using-DMA-example/m-p/1839545#M3707</link>
      <description>&lt;P&gt;it does not work&lt;/P&gt;</description>
      <pubDate>Tue, 02 Apr 2024 15:38:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Need-LPUART2-using-DMA-example/m-p/1839545#M3707</guid>
      <dc:creator>paulffffff</dc:creator>
      <dc:date>2024-04-02T15:38:16Z</dc:date>
    </item>
    <item>
      <title>Re: Need LPUART2 using DMA example.</title>
      <link>https://community.nxp.com/t5/S32-SDK/Need-LPUART2-using-DMA-example/m-p/1839583#M3708</link>
      <description>&lt;P&gt;assign channels 16 and 17 of DMA don't make it running&lt;/P&gt;</description>
      <pubDate>Tue, 02 Apr 2024 16:56:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Need-LPUART2-using-DMA-example/m-p/1839583#M3708</guid>
      <dc:creator>paulffffff</dc:creator>
      <dc:date>2024-04-02T16:56:15Z</dc:date>
    </item>
    <item>
      <title>Re: Need LPUART2 using DMA example.</title>
      <link>https://community.nxp.com/t5/S32-SDK/Need-LPUART2-using-DMA-example/m-p/1839747#M3710</link>
      <description>&lt;P&gt;Please test the modified project I sent you via private message.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 03 Apr 2024 01:55:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Need-LPUART2-using-DMA-example/m-p/1839747#M3710</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-04-03T01:55:58Z</dc:date>
    </item>
    <item>
      <title>Re: Need LPUART2 using DMA example.</title>
      <link>https://community.nxp.com/t5/S32-SDK/Need-LPUART2-using-DMA-example/m-p/1844305#M3717</link>
      <description>&lt;P&gt;can you create project DMA+ LPUART2?&lt;/P&gt;</description>
      <pubDate>Wed, 10 Apr 2024 19:42:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Need-LPUART2-using-DMA-example/m-p/1844305#M3717</guid>
      <dc:creator>paulffffff</dc:creator>
      <dc:date>2024-04-10T19:42:07Z</dc:date>
    </item>
    <item>
      <title>Re: Need LPUART2 using DMA example.</title>
      <link>https://community.nxp.com/t5/S32-SDK/Need-LPUART2-using-DMA-example/m-p/1844725#M3718</link>
      <description>&lt;P&gt;I tested it before sending it to you via private message last week. It can be built normally and the serial port information sent can be observed on the lpuart2_tx PTA9 pin. I'm using S32DS v3.5 + S32K3 RTD 3.0.0 D2303.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 11 Apr 2024 03:14:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Need-LPUART2-using-DMA-example/m-p/1844725#M3718</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-04-11T03:14:37Z</dc:date>
    </item>
  </channel>
</rss>