<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 SDK中的主题 Re: facing issue on CAN example code</title>
    <link>https://community.nxp.com/t5/S32-SDK/facing-issue-on-CAN-example-code/m-p/1776405#M3509</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;you can refer to&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-test-S32DS3-4/ta-p/1536225" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-test-S32DS3-4/ta-p/1536225&lt;/A&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Mon, 18 Dec 2023 12:38:31 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2023-12-18T12:38:31Z</dc:date>
    <item>
      <title>facing issue on CAN example code</title>
      <link>https://community.nxp.com/t5/S32-SDK/facing-issue-on-CAN-example-code/m-p/1775494#M3508</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;I am currently utilizing S32 Design Studio 3.4 and working with the S32K3 RTD AUTOSAR 4.4.2.0.0 D2203 example project. Specifically, I am attempting to implement the CAN example project, but I am encountering issues as it does not seem to be functioning correctly.Any configuration required kindly help me i am struck.&lt;BR /&gt;&lt;BR /&gt;Thanks and regards,&lt;BR /&gt;Rajasekar A&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 15 Dec 2023 09:33:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/facing-issue-on-CAN-example-code/m-p/1775494#M3508</guid>
      <dc:creator>selvarajasekar</dc:creator>
      <dc:date>2023-12-15T09:33:45Z</dc:date>
    </item>
    <item>
      <title>Re: facing issue on CAN example code</title>
      <link>https://community.nxp.com/t5/S32-SDK/facing-issue-on-CAN-example-code/m-p/1776405#M3509</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;you can refer to&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-test-S32DS3-4/ta-p/1536225" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-test-S32DS3-4/ta-p/1536225&lt;/A&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Mon, 18 Dec 2023 12:38:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/facing-issue-on-CAN-example-code/m-p/1776405#M3509</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-12-18T12:38:31Z</dc:date>
    </item>
  </channel>
</rss>