<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K118FTM组件输出PWM问题 in S32 SDK</title>
    <link>https://community.nxp.com/t5/S32-SDK/S32K118FTM%E7%BB%84%E4%BB%B6%E8%BE%93%E5%87%BAPWM%E9%97%AE%E9%A2%98/m-p/1669546#M3160</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;&lt;P&gt;Regarding your question…&lt;/P&gt;&lt;P&gt;&lt;EM&gt;[Google translation]&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;"S32K118FTM component output PWM problem&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;If you want to use a module of S32K118, such as FTM0, use its different channels, such as CH0 and CH5 to output PWM at different frequencies, how should it be implemented."&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;The FlexTimer Module (FTM) does not allow using different frequencies between channels of the same instance. If you need different PWM frequencies you will have to use different instances of FTM.&lt;/P&gt;&lt;P&gt;Hope it helps you.&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
    <pubDate>Wed, 14 Jun 2023 18:56:21 GMT</pubDate>
    <dc:creator>_Leo_</dc:creator>
    <dc:date>2023-06-14T18:56:21Z</dc:date>
    <item>
      <title>S32K118FTM组件输出PWM问题</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K118FTM%E7%BB%84%E4%BB%B6%E8%BE%93%E5%87%BAPWM%E9%97%AE%E9%A2%98/m-p/1668481#M3152</link>
      <description>&lt;P&gt;如果要使用S32K118的一个模组，例如FTM0，使用它的不同通道，如CH0和CH5输出不同频率输出PWM，应该如何实现。&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jun 2023 14:40:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K118FTM%E7%BB%84%E4%BB%B6%E8%BE%93%E5%87%BAPWM%E9%97%AE%E9%A2%98/m-p/1668481#M3152</guid>
      <dc:creator>GAC-Lamp-Knight</dc:creator>
      <dc:date>2023-06-13T14:40:24Z</dc:date>
    </item>
    <item>
      <title>Re: S32K118FTM组件输出PWM问题</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K118FTM%E7%BB%84%E4%BB%B6%E8%BE%93%E5%87%BAPWM%E9%97%AE%E9%A2%98/m-p/1669546#M3160</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;&lt;P&gt;Regarding your question…&lt;/P&gt;&lt;P&gt;&lt;EM&gt;[Google translation]&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;"S32K118FTM component output PWM problem&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;If you want to use a module of S32K118, such as FTM0, use its different channels, such as CH0 and CH5 to output PWM at different frequencies, how should it be implemented."&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;The FlexTimer Module (FTM) does not allow using different frequencies between channels of the same instance. If you need different PWM frequencies you will have to use different instances of FTM.&lt;/P&gt;&lt;P&gt;Hope it helps you.&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Wed, 14 Jun 2023 18:56:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K118FTM%E7%BB%84%E4%BB%B6%E8%BE%93%E5%87%BAPWM%E9%97%AE%E9%A2%98/m-p/1669546#M3160</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2023-06-14T18:56:21Z</dc:date>
    </item>
  </channel>
</rss>