<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Crypto in S32 SDK</title>
    <link>https://community.nxp.com/t5/S32-SDK/Crypto/m-p/1667265#M3147</link>
    <description>&lt;P&gt;&lt;SPAN&gt;I am currently using the S32K144 for information security development and would like to ask how to use address mode when calculating MAC values using the MCAL version.&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;&lt;SPAN&gt;When I used the SDK version, there was a function called Csec_Ip_GenerateMacAddrMode that could be implemented, but it wasn't found in the MCAL version.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;我现在在使用S32K144做信息安全开发，想问一下在使用MCAL版本计算MAC值时，如何使用地址模式。&lt;/P&gt;&lt;P&gt;我在使用SDK版本时，有一函数Csec_Ip_GenerateMacAddrMode可以实现，但是在MCAL版本中并未找到。&lt;/P&gt;</description>
    <pubDate>Sun, 11 Jun 2023 07:23:43 GMT</pubDate>
    <dc:creator>严雷</dc:creator>
    <dc:date>2023-06-11T07:23:43Z</dc:date>
    <item>
      <title>Crypto</title>
      <link>https://community.nxp.com/t5/S32-SDK/Crypto/m-p/1667265#M3147</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I am currently using the S32K144 for information security development and would like to ask how to use address mode when calculating MAC values using the MCAL version.&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;&lt;SPAN&gt;When I used the SDK version, there was a function called Csec_Ip_GenerateMacAddrMode that could be implemented, but it wasn't found in the MCAL version.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;我现在在使用S32K144做信息安全开发，想问一下在使用MCAL版本计算MAC值时，如何使用地址模式。&lt;/P&gt;&lt;P&gt;我在使用SDK版本时，有一函数Csec_Ip_GenerateMacAddrMode可以实现，但是在MCAL版本中并未找到。&lt;/P&gt;</description>
      <pubDate>Sun, 11 Jun 2023 07:23:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Crypto/m-p/1667265#M3147</guid>
      <dc:creator>严雷</dc:creator>
      <dc:date>2023-06-11T07:23:43Z</dc:date>
    </item>
    <item>
      <title>Re: Crypto</title>
      <link>https://community.nxp.com/t5/S32-SDK/Crypto/m-p/1681996#M3180</link>
      <description>&lt;P&gt;&lt;SPAN class="uiOutputText"&gt;RTD produce supports both MCAL and SDK. So you can use RTD like what you did on SDK version (it means RTD also provides Csec_Ip_GenerateMacAddrMode function like what you have on SDK version)&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="uiOutputText"&gt;Please let me know if you need more details for this or you still want to use using from MCAL API.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jul 2023 11:39:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Crypto/m-p/1681996#M3180</guid>
      <dc:creator>CongDang</dc:creator>
      <dc:date>2023-07-05T11:39:24Z</dc:date>
    </item>
  </channel>
</rss>