<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 SDKのトピックRe: About API Siul2_Port_Ip_SetPinDirection</title>
    <link>https://community.nxp.com/t5/S32-SDK/About-API-Siul2-Port-Ip-SetPinDirection/m-p/1654473#M3093</link>
    <description>&lt;P&gt;&lt;A href="mailto:Hi@jetty1024" target="_blank"&gt;Hi@jetty1024&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;yes ,you can use this function to change GPIO direction.&lt;/P&gt;
&lt;P&gt;you can read this function then you will easily find that,set 0 -&amp;gt;In,set 1-&amp;gt;Out&lt;/P&gt;</description>
    <pubDate>Mon, 22 May 2023 06:56:32 GMT</pubDate>
    <dc:creator>Senlent</dc:creator>
    <dc:date>2023-05-22T06:56:32Z</dc:date>
    <item>
      <title>About API Siul2_Port_Ip_SetPinDirection</title>
      <link>https://community.nxp.com/t5/S32-SDK/About-API-Siul2-Port-Ip-SetPinDirection/m-p/1654297#M3092</link>
      <description>&lt;P&gt;So if I set a GPIO direction as 'Input' in the pin configuration. And I want to change its direction to 'Output' at some time during the program is running.&lt;/P&gt;&lt;P&gt;Should I use the API below?&lt;/P&gt;&lt;DIV&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jetty1012_0-1684724088345.jpeg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/224097iC4F255C761152175/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jetty1012_0-1684724088345.jpeg" alt="jetty1012_0-1684724088345.jpeg" /&gt;&lt;/span&gt;&lt;P&gt;If so, should I set the 3rd param as 0 or 1 for 'Output'? Is there any manual about this?&lt;/P&gt;&lt;P&gt;I'm using S32K312 RTD v2.0.1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jetty&lt;/P&gt;&lt;/DIV&gt;</description>
      <pubDate>Mon, 22 May 2023 03:01:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/About-API-Siul2-Port-Ip-SetPinDirection/m-p/1654297#M3092</guid>
      <dc:creator>jetty1012</dc:creator>
      <dc:date>2023-05-22T03:01:55Z</dc:date>
    </item>
    <item>
      <title>Re: About API Siul2_Port_Ip_SetPinDirection</title>
      <link>https://community.nxp.com/t5/S32-SDK/About-API-Siul2-Port-Ip-SetPinDirection/m-p/1654473#M3093</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@jetty1024" target="_blank"&gt;Hi@jetty1024&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;yes ,you can use this function to change GPIO direction.&lt;/P&gt;
&lt;P&gt;you can read this function then you will easily find that,set 0 -&amp;gt;In,set 1-&amp;gt;Out&lt;/P&gt;</description>
      <pubDate>Mon, 22 May 2023 06:56:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/About-API-Siul2-Port-Ip-SetPinDirection/m-p/1654473#M3093</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2023-05-22T06:56:32Z</dc:date>
    </item>
  </channel>
</rss>