<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K148 PDB ADC in S32 SDK</title>
    <link>https://community.nxp.com/t5/S32-SDK/S32K148-PDB-ADC/m-p/1547346#M2771</link>
    <description>&lt;P&gt;HI：&lt;/P&gt;&lt;P&gt;When I configure the BACK-TO-BACK mode of PDB, can I only configure channels 0-7 in sequence, but not remove channels from the middle ？&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 02 Nov 2022 03:12:16 GMT</pubDate>
    <dc:creator>QJ_HAPPY</dc:creator>
    <dc:date>2022-11-02T03:12:16Z</dc:date>
    <item>
      <title>S32K148 PDB ADC</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K148-PDB-ADC/m-p/1547346#M2771</link>
      <description>&lt;P&gt;HI：&lt;/P&gt;&lt;P&gt;When I configure the BACK-TO-BACK mode of PDB, can I only configure channels 0-7 in sequence, but not remove channels from the middle ？&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Nov 2022 03:12:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K148-PDB-ADC/m-p/1547346#M2771</guid>
      <dc:creator>QJ_HAPPY</dc:creator>
      <dc:date>2022-11-02T03:12:16Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148 PDB ADC</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K148-PDB-ADC/m-p/1547489#M2772</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Please read the "46.1.3 Back-to-back acknowledgement connections" and "Figure 46-5. PDB-ADC back to back con":&amp;nbsp;&lt;/SPAN&gt;&lt;EM&gt;Back-to-back operation enables the ADC conversions complete to trigger the &lt;STRONG&gt;next&lt;/STRONG&gt; PDB channel pre-trigger and trigger output.&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Back-to-back acknowledgement connections.png" style="width: 542px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/198862i602661F0E1DC8095/image-size/large?v=v2&amp;amp;px=999" role="button" title="Back-to-back acknowledgement connections.png" alt="Back-to-back acknowledgement connections.png" /&gt;&lt;/span&gt;&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;There is no such possibility that Pre-trigger 0 COCO is directly connected to Pre-trigger 2.&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Figure 46-5. PDB-ADC back to back connection.png" style="width: 798px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/198865iA53F56D16DF029DF/image-size/large?v=v2&amp;amp;px=999" role="button" title="Figure 46-5. PDB-ADC back to back connection.png" alt="Figure 46-5. PDB-ADC back to back connection.png" /&gt;&lt;/span&gt;&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 02 Nov 2022 06:58:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K148-PDB-ADC/m-p/1547489#M2772</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-11-02T06:58:23Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148 PDB ADC</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K148-PDB-ADC/m-p/1548664#M2776</link>
      <description>I understand now. Thank you for your reply</description>
      <pubDate>Fri, 04 Nov 2022 05:13:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K148-PDB-ADC/m-p/1548664#M2776</guid>
      <dc:creator>QJ_HAPPY</dc:creator>
      <dc:date>2022-11-04T05:13:43Z</dc:date>
    </item>
  </channel>
</rss>