<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32G LLCE (CAN) excute command return LLCE_ERROR_COMMAND_NOTACCEPTED in S32 SDK</title>
    <link>https://community.nxp.com/t5/S32-SDK/S32G-LLCE-CAN-excute-command-return-LLCE-ERROR-COMMAND/m-p/1538547#M2736</link>
    <description>&lt;P&gt;Dear All&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;At moment, I am using LLCE firmware and driver which is from NXP in FreeRTOS, I met a issuse that the LLCE return&amp;nbsp;LLCE_ERROR_COMMAND_NOTACCEPTED when I call some LLCE routines.&lt;/P&gt;&lt;P&gt;The sisuation is that&lt;/P&gt;&lt;P&gt;1 . send a "set controller mode command"&amp;nbsp; immediately after send a "write a message command"&amp;nbsp; &amp;nbsp;in one task .&lt;/P&gt;&lt;P&gt;2 . event when I seprate them in two task (each task cycle is 1ms),&amp;nbsp; I met the same issue.&lt;/P&gt;&lt;P&gt;Very hope to recieve your answers , thank you very much !&lt;/P&gt;</description>
    <pubDate>Mon, 17 Oct 2022 12:04:33 GMT</pubDate>
    <dc:creator>chenhong</dc:creator>
    <dc:date>2022-10-17T12:04:33Z</dc:date>
    <item>
      <title>S32G LLCE (CAN) excute command return LLCE_ERROR_COMMAND_NOTACCEPTED</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32G-LLCE-CAN-excute-command-return-LLCE-ERROR-COMMAND/m-p/1538547#M2736</link>
      <description>&lt;P&gt;Dear All&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;At moment, I am using LLCE firmware and driver which is from NXP in FreeRTOS, I met a issuse that the LLCE return&amp;nbsp;LLCE_ERROR_COMMAND_NOTACCEPTED when I call some LLCE routines.&lt;/P&gt;&lt;P&gt;The sisuation is that&lt;/P&gt;&lt;P&gt;1 . send a "set controller mode command"&amp;nbsp; immediately after send a "write a message command"&amp;nbsp; &amp;nbsp;in one task .&lt;/P&gt;&lt;P&gt;2 . event when I seprate them in two task (each task cycle is 1ms),&amp;nbsp; I met the same issue.&lt;/P&gt;&lt;P&gt;Very hope to recieve your answers , thank you very much !&lt;/P&gt;</description>
      <pubDate>Mon, 17 Oct 2022 12:04:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32G-LLCE-CAN-excute-command-return-LLCE-ERROR-COMMAND/m-p/1538547#M2736</guid>
      <dc:creator>chenhong</dc:creator>
      <dc:date>2022-10-17T12:04:33Z</dc:date>
    </item>
    <item>
      <title>Re: S32G LLCE (CAN) excute command return LLCE_ERROR_COMMAND_NOTACCEPTED</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32G-LLCE-CAN-excute-command-return-LLCE-ERROR-COMMAND/m-p/1568180#M2845</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/207630"&gt;@chenhong&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;When you send the "Set Controller Mode Command", the LLCE controller will issue a notification of its state in the "Set Controller Mode notification" command. Have you checked the controller state before writing a message to it?&lt;/P&gt;
&lt;P&gt;Also, Can you try to increase the delay of the&amp;nbsp;&lt;SPAN&gt;write a message command thread from 1 ms to 10 ms or even more&lt;/SPAN&gt;?&lt;/P&gt;
&lt;P&gt;Let us know if it doesn't work.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Mayank s Patel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 12 Dec 2022 09:49:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32G-LLCE-CAN-excute-command-return-LLCE-ERROR-COMMAND/m-p/1568180#M2845</guid>
      <dc:creator>MayanksPatel</dc:creator>
      <dc:date>2022-12-12T09:49:11Z</dc:date>
    </item>
  </channel>
</rss>