<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 SDKのトピックRe: S32K FLEXRAM EEPROM</title>
    <link>https://community.nxp.com/t5/S32-SDK/S32K-FLEXRAM-EEPROM/m-p/1528476#M2718</link>
    <description>&lt;P&gt;hi , have you got any solution? I met the same problem and could you pls share the solution?&lt;/P&gt;</description>
    <pubDate>Tue, 27 Sep 2022 02:58:14 GMT</pubDate>
    <dc:creator>JustVb</dc:creator>
    <dc:date>2022-09-27T02:58:14Z</dc:date>
    <item>
      <title>S32K FLEXRAM EEPROM</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K-FLEXRAM-EEPROM/m-p/1481545#M2564</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &lt;SPAN&gt;Currently there is a problem in using S32K144，&lt;/SPAN&gt;&lt;SPAN&gt;in case of setting FlexNVM is 32k d-flash(Base addr:0x10000000) and 32k e-flash(Base addr:0x10008000), setting FlexRAM is 4k EEE(Base addr:0x14000000)。d-flash is used to save calibration data，e-flash is used to save DID and DTC and other data(Such as the application program valid flag)。How do I store the initial value of DID in EEPROM。How do I store a valid flag&amp;nbsp; for an application program in EEPROM。&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Method 1：&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I want to write into&amp;nbsp;e-flash by using JFLASH SWD。&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Method 2：&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The runtime checks if the initial value has been written, and if not, writes。&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;but&amp;nbsp;a valid flag&amp;nbsp; for an application must be written&amp;nbsp;together with the application program，because bootloader program need to judge the flag to determine&amp;nbsp;whether to jump to&amp;nbsp;application program。&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The address of valid flag&amp;nbsp; for an application is 0x14000000,but JFLASH cannot program the address,but can program address from 0x10000000 to 0x1000FFFF. I want to kown address&amp;nbsp;0x14000000 map to&amp;nbsp;Which address&amp;nbsp;from 0x10000000 to 0x1000FFFF.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 29 Jun 2022 05:20:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K-FLEXRAM-EEPROM/m-p/1481545#M2564</guid>
      <dc:creator>chenze</dc:creator>
      <dc:date>2022-06-29T05:20:59Z</dc:date>
    </item>
    <item>
      <title>Re: S32K FLEXRAM EEPROM</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K-FLEXRAM-EEPROM/m-p/1528476#M2718</link>
      <description>&lt;P&gt;hi , have you got any solution? I met the same problem and could you pls share the solution?&lt;/P&gt;</description>
      <pubDate>Tue, 27 Sep 2022 02:58:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K-FLEXRAM-EEPROM/m-p/1528476#M2718</guid>
      <dc:creator>JustVb</dc:creator>
      <dc:date>2022-09-27T02:58:14Z</dc:date>
    </item>
  </channel>
</rss>