<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K1 edge sensitive interrupt on GPIO using RTD in S32 SDK</title>
    <link>https://community.nxp.com/t5/S32-SDK/S32K1-edge-sensitive-interrupt-on-GPIO-using-RTD/m-p/1522328#M2703</link>
    <description>&lt;P&gt;Unfortunately, this stopped working after RTD version 4.4.1.0.0 (D2108).&lt;/P&gt;&lt;P&gt;Is there a way to create an edge sensitive GPIO interrupt with the RTDs on newer releases?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 14 Sep 2022 22:48:26 GMT</pubDate>
    <dc:creator>hns80</dc:creator>
    <dc:date>2022-09-14T22:48:26Z</dc:date>
    <item>
      <title>S32K1 edge sensitive interrupt on GPIO using RTD</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K1-edge-sensitive-interrupt-on-GPIO-using-RTD/m-p/1438559#M2478</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Is there a way to use the peripheral or pin perspective to enable a rising or falling edge interrupt on a GPIO using the low level driver (not the mcal)?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;If not, is there an RTD function call that can do it, or does this need to be done by directly writing the pin control register? I searched the RTDs and didn't see anything that did it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 05 Apr 2022 00:18:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K1-edge-sensitive-interrupt-on-GPIO-using-RTD/m-p/1438559#M2478</guid>
      <dc:creator>hns80</dc:creator>
      <dc:date>2022-04-05T00:18:54Z</dc:date>
    </item>
    <item>
      <title>Re: S32K1 edge sensitive interrupt on GPIO using RTD</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K1-edge-sensitive-interrupt-on-GPIO-using-RTD/m-p/1440439#M2490</link>
      <description>&lt;P&gt;Hello Jeff,&lt;/P&gt;
&lt;P&gt;In Port_Ci_Port_Ip.c of Port_Ip&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_2-1649323747801.png" style="width: 324px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/176220i5D155875995E1415/image-dimensions/324x208?v=v2" width="324" height="208" role="button" title="danielmartynek_2-1649323747801.png" alt="danielmartynek_2-1649323747801.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielmartynek_2-1649323747801.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;there are functions for reading and writing the PCR registers.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1649323448158.png" style="width: 714px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/176218i9C1E68CC94D18D38/image-dimensions/714x496?v=v2" width="714" height="496" role="button" title="danielmartynek_0-1649323448158.png" alt="danielmartynek_0-1649323448158.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielmartynek_0-1649323448158.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_1-1649323480836.png" style="width: 635px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/176219i3F6853860774AA01/image-dimensions/635x338?v=v2" width="635" height="338" role="button" title="danielmartynek_1-1649323480836.png" alt="danielmartynek_1-1649323480836.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielmartynek_1-1649323480836.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="uiOutputText"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 07 Apr 2022 09:29:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K1-edge-sensitive-interrupt-on-GPIO-using-RTD/m-p/1440439#M2490</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2022-04-07T09:29:54Z</dc:date>
    </item>
    <item>
      <title>Re: S32K1 edge sensitive interrupt on GPIO using RTD</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K1-edge-sensitive-interrupt-on-GPIO-using-RTD/m-p/1522328#M2703</link>
      <description>&lt;P&gt;Unfortunately, this stopped working after RTD version 4.4.1.0.0 (D2108).&lt;/P&gt;&lt;P&gt;Is there a way to create an edge sensitive GPIO interrupt with the RTDs on newer releases?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Sep 2022 22:48:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K1-edge-sensitive-interrupt-on-GPIO-using-RTD/m-p/1522328#M2703</guid>
      <dc:creator>hns80</dc:creator>
      <dc:date>2022-09-14T22:48:26Z</dc:date>
    </item>
  </channel>
</rss>