<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 SDKのトピックRe: S32DS examples compile issue</title>
    <link>https://community.nxp.com/t5/S32-SDK/S32DS-examples-compile-issue/m-p/652370#M27</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;It seems like generated files from Processor Expert do not exist.&lt;/P&gt;&lt;P&gt;I'd recommend you to generate the processor expert code first since build process does not trigger the code generator.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/1942i5B603B38D15BAD76/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;When the generation is done you should see the new project folder "Generated Code" which includes e.g. "cpu.h" that was missing when you initially compiled main.c.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now you can build the project and at the end of the process you should see executable elf file being created:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2020i1601B5CA3E30C608/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Oct 2016 14:21:55 GMT</pubDate>
    <dc:creator>stanish</dc:creator>
    <dc:date>2016-10-04T14:21:55Z</dc:date>
    <item>
      <title>S32DS examples compile issue</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32DS-examples-compile-issue/m-p/652369#M26</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have problem on compiling when imported the examples.&lt;/P&gt;&lt;P&gt;here is my log:&lt;/P&gt;&lt;P&gt;arm-none-eabi-gcc -DCPU_S32K144HFT0VLLT -DS32K -I"E:\workspace\FreeRTOS_Example\Sources" -I"d:\Freescale\S32_ARM_v1.2\S32DS\S32_SDK_EAR_0.8.1/examples/demo_apps/FreeRTOS/sources" -I"d:\Freescale\S32_ARM_v1.2\S32DS\S32_SDK_EAR_0.8.1/rtos/FreeRTOS/Source/include" -I"d:\Freescale\S32_ARM_v1.2\S32DS\S32_SDK_EAR_0.8.1/rtos/FreeRTOS/Source/portable/MemMang" -I"d:\Freescale\S32_ARM_v1.2\S32DS\S32_SDK_EAR_0.8.1/rtos/FreeRTOS/Source/portable/GCC/ARM_CM4F" -I"d:\Freescale\S32_ARM_v1.2\S32DS\S32_SDK_EAR_0.8.1/platform/devices/S32K144/include" -I"d:\Freescale\S32_ARM_v1.2\S32DS\S32_SDK_EAR_0.8.1/platform/devices/S32K144" -I"d:\Freescale\S32_ARM_v1.2\S32DS\S32_SDK_EAR_0.8.1/platform/devices" -I"d:\Freescale\S32_ARM_v1.2\S32DS\S32_SDK_EAR_0.8.1/platform/hal/inc" -I"d:\Freescale\S32_ARM_v1.2\S32DS\S32_SDK_EAR_0.8.1/platform/drivers/inc" -O0 -g3 -Wall -c -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections -mcpu=cortex-m4 -mthumb -mfloat-abi=softfp -mfpu=fpv4-sp-d16 -specs=nano.specs -specs=nosys.specs --sysroot="D:\Freescale\S32_ARM_v1.2\eclipse\../Cross_Tools/gcc-arm-none-eabi-4_9/arm-none-eabi/newlib" -MMD -MP -MF"Sources/main.d" -MT"Sources/main.o" -c -o "Sources/main.o" "../Sources/main.c"&lt;BR /&gt;../Sources/main.c:61:17: fatal error: Cpu.h: No such file or directory&lt;BR /&gt; #include "Cpu.h"&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Sep 2016 12:13:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32DS-examples-compile-issue/m-p/652369#M26</guid>
      <dc:creator>weisenzhang</dc:creator>
      <dc:date>2016-09-26T12:13:21Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS examples compile issue</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32DS-examples-compile-issue/m-p/652370#M27</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;It seems like generated files from Processor Expert do not exist.&lt;/P&gt;&lt;P&gt;I'd recommend you to generate the processor expert code first since build process does not trigger the code generator.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/1942i5B603B38D15BAD76/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;When the generation is done you should see the new project folder "Generated Code" which includes e.g. "cpu.h" that was missing when you initially compiled main.c.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now you can build the project and at the end of the process you should see executable elf file being created:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2020i1601B5CA3E30C608/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Oct 2016 14:21:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32DS-examples-compile-issue/m-p/652370#M27</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2016-10-04T14:21:55Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS examples compile issue</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32DS-examples-compile-issue/m-p/652371#M28</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thanks, Stan, that's right, it works now.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Oct 2016 00:16:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32DS-examples-compile-issue/m-p/652371#M28</guid>
      <dc:creator>weisenzhang</dc:creator>
      <dc:date>2016-10-06T00:16:55Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS examples compile issue</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32DS-examples-compile-issue/m-p/652372#M29</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Aug 2017 07:13:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32DS-examples-compile-issue/m-p/652372#M29</guid>
      <dc:creator>taehokwon</dc:creator>
      <dc:date>2017-08-03T07:13:37Z</dc:date>
    </item>
  </channel>
</rss>