<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K1 SPI interrupt with RTD in S32 SDK</title>
    <link>https://community.nxp.com/t5/S32-SDK/S32K1-SPI-interrupt-with-RTD/m-p/1433714#M2462</link>
    <description>&lt;P&gt;I'm trying to modify the Lpspi_Ip_InternalLoopback example to create an interrupt at the end of transmission.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can see that the&amp;nbsp;Lpspi_Ip_ConfigType has a field to enable the interrupt with&amp;nbsp;LPSPI_IP_INTERRUPT.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I do not see any way to enable the interrupt through the peripheral perspective for the SPI driver. Is there a way to enable the interrupt without manually editing the generated code?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="hns80_0-1648166945214.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/174774i3DD0B5E26934DE15/image-size/medium?v=v2&amp;amp;px=400" role="button" title="hns80_0-1648166945214.png" alt="hns80_0-1648166945214.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 25 Mar 2022 00:12:04 GMT</pubDate>
    <dc:creator>hns80</dc:creator>
    <dc:date>2022-03-25T00:12:04Z</dc:date>
    <item>
      <title>S32K1 SPI interrupt with RTD</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K1-SPI-interrupt-with-RTD/m-p/1433714#M2462</link>
      <description>&lt;P&gt;I'm trying to modify the Lpspi_Ip_InternalLoopback example to create an interrupt at the end of transmission.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can see that the&amp;nbsp;Lpspi_Ip_ConfigType has a field to enable the interrupt with&amp;nbsp;LPSPI_IP_INTERRUPT.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I do not see any way to enable the interrupt through the peripheral perspective for the SPI driver. Is there a way to enable the interrupt without manually editing the generated code?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="hns80_0-1648166945214.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/174774i3DD0B5E26934DE15/image-size/medium?v=v2&amp;amp;px=400" role="button" title="hns80_0-1648166945214.png" alt="hns80_0-1648166945214.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 25 Mar 2022 00:12:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K1-SPI-interrupt-with-RTD/m-p/1433714#M2462</guid>
      <dc:creator>hns80</dc:creator>
      <dc:date>2022-03-25T00:12:04Z</dc:date>
    </item>
    <item>
      <title>Re: S32K1 SPI interrupt with RTD</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K1-SPI-interrupt-with-RTD/m-p/1433843#M2463</link>
      <description>&lt;P&gt;Hi hns80,&lt;/P&gt;
&lt;P&gt;Sorry for the inconvenience we bring you!&amp;nbsp;&lt;BR /&gt;There is currently no way to enable interrupts from the SPI driver's peripheral perspective. This problem has been reported in the system.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;IP driver will be in &lt;STRONG&gt;POLLING&lt;/STRONG&gt; mode after initialize as default mode, if you want to change to other mode&amp;nbsp;&lt;STRONG&gt;Lpspi_Ip_UpdateTransferMode&lt;/STRONG&gt;() should be used.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 25 Mar 2022 05:06:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K1-SPI-interrupt-with-RTD/m-p/1433843#M2463</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-03-25T05:06:19Z</dc:date>
    </item>
  </channel>
</rss>