<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 SDK中的主题 S32K146 eDma transfer</title>
    <link>https://community.nxp.com/t5/S32-SDK/S32K146-eDma-transfer/m-p/1413617#M2419</link>
    <description>&lt;P&gt;Hi all, I need to implement a dma transfer from memory to a register, triggered by a timer. The platform is a S32K146 with S32DS 3.4 and SDK 4.0.2. I tried to modify the "edma_transfer_s32k146" example in order to setup the FlexTimer FTM1 - channel 1 as a PWM generator (checking the "External Trigger" box) and setting the EDMA field "Channel Request" on EDMA_REQ_FTM1_CNANNEL_1 value.&lt;/P&gt;&lt;P&gt;In the source code I simply added a call to start the DMA channel&lt;/P&gt;&lt;P&gt;EDMA_DRV_StartChannel(dmaControllerChn0_Config.virtChnConfig);&lt;/P&gt;&lt;P&gt;Could someone give me any advice to make this working? Is there, on the Net, any example on using DMA driven by a timer? Should I use the TRGMUX module?&lt;/P&gt;&lt;P&gt;Thank you all in advance.&lt;/P&gt;&lt;P&gt;Alberto&lt;/P&gt;</description>
    <pubDate>Tue, 15 Feb 2022 10:23:02 GMT</pubDate>
    <dc:creator>albertoferrero</dc:creator>
    <dc:date>2022-02-15T10:23:02Z</dc:date>
    <item>
      <title>S32K146 eDma transfer</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K146-eDma-transfer/m-p/1413617#M2419</link>
      <description>&lt;P&gt;Hi all, I need to implement a dma transfer from memory to a register, triggered by a timer. The platform is a S32K146 with S32DS 3.4 and SDK 4.0.2. I tried to modify the "edma_transfer_s32k146" example in order to setup the FlexTimer FTM1 - channel 1 as a PWM generator (checking the "External Trigger" box) and setting the EDMA field "Channel Request" on EDMA_REQ_FTM1_CNANNEL_1 value.&lt;/P&gt;&lt;P&gt;In the source code I simply added a call to start the DMA channel&lt;/P&gt;&lt;P&gt;EDMA_DRV_StartChannel(dmaControllerChn0_Config.virtChnConfig);&lt;/P&gt;&lt;P&gt;Could someone give me any advice to make this working? Is there, on the Net, any example on using DMA driven by a timer? Should I use the TRGMUX module?&lt;/P&gt;&lt;P&gt;Thank you all in advance.&lt;/P&gt;&lt;P&gt;Alberto&lt;/P&gt;</description>
      <pubDate>Tue, 15 Feb 2022 10:23:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K146-eDma-transfer/m-p/1413617#M2419</guid>
      <dc:creator>albertoferrero</dc:creator>
      <dc:date>2022-02-15T10:23:02Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 eDma transfer</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K146-eDma-transfer/m-p/1414331#M2421</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/150195"&gt;@albertoferrero&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;You can refer to this example:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K118-FTM-PWM-DMA-S32DS-2-2/ta-p/1342183" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K118-FTM-PWM-DMA-S32DS-2-2/ta-p/1342183&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 16 Feb 2022 09:35:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K146-eDma-transfer/m-p/1414331#M2421</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2022-02-16T09:35:36Z</dc:date>
    </item>
  </channel>
</rss>