<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 SDK中的主题 S32k SDK build Project Name change</title>
    <link>https://community.nxp.com/t5/S32-SDK/S32k-SDK-build-Project-Name-change/m-p/1364544#M2310</link>
    <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;HI,&lt;BR /&gt;&amp;nbsp; In s32 SDK the build project creates a .elf, with projectname.elf as default.&lt;/P&gt;&lt;P&gt;But is there any way, without changing the projects name&lt;BR /&gt;I want to have the .elf name, of my choice ? I do not want to rename pressing F2, instead when I give build project it should generate the .hex/.ellf&amp;nbsp; with name of my choice. Is there a way to do this ?&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;BR /&gt;Abhijith Shankar&lt;/P&gt;</description>
    <pubDate>Mon, 01 Nov 2021 12:02:16 GMT</pubDate>
    <dc:creator>abhijithshankaren</dc:creator>
    <dc:date>2021-11-01T12:02:16Z</dc:date>
    <item>
      <title>S32k SDK build Project Name change</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32k-SDK-build-Project-Name-change/m-p/1364544#M2310</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;HI,&lt;BR /&gt;&amp;nbsp; In s32 SDK the build project creates a .elf, with projectname.elf as default.&lt;/P&gt;&lt;P&gt;But is there any way, without changing the projects name&lt;BR /&gt;I want to have the .elf name, of my choice ? I do not want to rename pressing F2, instead when I give build project it should generate the .hex/.ellf&amp;nbsp; with name of my choice. Is there a way to do this ?&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;BR /&gt;Abhijith Shankar&lt;/P&gt;</description>
      <pubDate>Mon, 01 Nov 2021 12:02:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32k-SDK-build-Project-Name-change/m-p/1364544#M2310</guid>
      <dc:creator>abhijithshankaren</dc:creator>
      <dc:date>2021-11-01T12:02:16Z</dc:date>
    </item>
    <item>
      <title>Re: S32k SDK build Project Name change</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32k-SDK-build-Project-Name-change/m-p/1364765#M2311</link>
      <description>&lt;P&gt;Hi&amp;nbsp;Abhijith Shankar,&lt;/P&gt;
&lt;P&gt;You can change the name of elf file in Build Artifact tab:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Artifact name.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/160891i4FFF831AE25CEA29/image-size/large?v=v2&amp;amp;px=999" role="button" title="Artifact name.png" alt="Artifact name.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Artifact name.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Nov 2021 02:14:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32k-SDK-build-Project-Name-change/m-p/1364765#M2311</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2021-11-02T02:14:12Z</dc:date>
    </item>
  </channel>
</rss>