<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K148 IAR - print 64bit values in S32 SDK</title>
    <link>https://community.nxp.com/t5/S32-SDK/S32K148-IAR-print-64bit-values/m-p/1355025#M2294</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Does IAR compiler for S32K148 support printing 64bit integers (%lld, %llu, %llx) with snprintf() function?&lt;/P&gt;&lt;P&gt;I have a strange behavior in my application. When I add one global uint32_t variable, then snprintf() prints 64bit integers with %lld incorrectly (shifted). When I remove this additional variable or add one more global uint32_t then it prints the 64-bt int with %lld correctly.&lt;/P&gt;&lt;P&gt;32-bit integers are printed correctly in both cases.&lt;/P&gt;&lt;P&gt;Any idea what could be the cause?&lt;/P&gt;</description>
    <pubDate>Wed, 13 Oct 2021 13:31:59 GMT</pubDate>
    <dc:creator>jakub_mielczare</dc:creator>
    <dc:date>2021-10-13T13:31:59Z</dc:date>
    <item>
      <title>S32K148 IAR - print 64bit values</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K148-IAR-print-64bit-values/m-p/1355025#M2294</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Does IAR compiler for S32K148 support printing 64bit integers (%lld, %llu, %llx) with snprintf() function?&lt;/P&gt;&lt;P&gt;I have a strange behavior in my application. When I add one global uint32_t variable, then snprintf() prints 64bit integers with %lld incorrectly (shifted). When I remove this additional variable or add one more global uint32_t then it prints the 64-bt int with %lld correctly.&lt;/P&gt;&lt;P&gt;32-bit integers are printed correctly in both cases.&lt;/P&gt;&lt;P&gt;Any idea what could be the cause?&lt;/P&gt;</description>
      <pubDate>Wed, 13 Oct 2021 13:31:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K148-IAR-print-64bit-values/m-p/1355025#M2294</guid>
      <dc:creator>jakub_mielczare</dc:creator>
      <dc:date>2021-10-13T13:31:59Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148 IAR - print 64bit values</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K148-IAR-print-64bit-values/m-p/1356343#M2295</link>
      <description>&lt;P&gt;Hi Jakub,&lt;/P&gt;
&lt;P&gt;after short discussion with our S32DS expert, our recommendation is to forward this to IAR as we can't help here.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Fri, 15 Oct 2021 08:50:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K148-IAR-print-64bit-values/m-p/1356343#M2295</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2021-10-15T08:50:39Z</dc:date>
    </item>
  </channel>
</rss>