<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K148 LWIP RTM v3.0.0 example in S32 SDK</title>
    <link>https://community.nxp.com/t5/S32-SDK/S32K148-LWIP-RTM-v3-0-0-example/m-p/1325962#M2266</link>
    <description>&lt;P&gt;example:lwip_s32K148&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I'll look at the code for this example,I have ported LWIP protocol on 5748 before，In contrast, there are some questions。&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;When self-porting, the interface corresponding to the low driver is:low_level_output 、low_level_input、low_level_input.&amp;nbsp; in function low_level_input,Initializing a network adapter.but int the lwip_S32k148,i just found function: 'enetif_low_level_output'、'enetif_low_level_init',don't found about filed ' low_level_input'? where do i found this function.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;i check help doc 'lwip_s32k148_group.html',but hasn't any introduce.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;in this example, enet recevie data ,dose trigger interrupt?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I want use MQTT protocal,dose has any example?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 19 Aug 2021 08:16:09 GMT</pubDate>
    <dc:creator>liuweiliang</dc:creator>
    <dc:date>2021-08-19T08:16:09Z</dc:date>
    <item>
      <title>S32K148 LWIP RTM v3.0.0 example</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K148-LWIP-RTM-v3-0-0-example/m-p/1325962#M2266</link>
      <description>&lt;P&gt;example:lwip_s32K148&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I'll look at the code for this example,I have ported LWIP protocol on 5748 before，In contrast, there are some questions。&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;When self-porting, the interface corresponding to the low driver is:low_level_output 、low_level_input、low_level_input.&amp;nbsp; in function low_level_input,Initializing a network adapter.but int the lwip_S32k148,i just found function: 'enetif_low_level_output'、'enetif_low_level_init',don't found about filed ' low_level_input'? where do i found this function.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;i check help doc 'lwip_s32k148_group.html',but hasn't any introduce.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;in this example, enet recevie data ,dose trigger interrupt?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I want use MQTT protocal,dose has any example?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 19 Aug 2021 08:16:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K148-LWIP-RTM-v3-0-0-example/m-p/1325962#M2266</guid>
      <dc:creator>liuweiliang</dc:creator>
      <dc:date>2021-08-19T08:16:09Z</dc:date>
    </item>
  </channel>
</rss>