<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 SDKのトピックRe: S32K144 SPI half-duplex DMA</title>
    <link>https://community.nxp.com/t5/S32-SDK/S32K144-SPI-half-duplex-DMA/m-p/712519#M218</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your feedback.&lt;/P&gt;&lt;P&gt;We know that is a problem&amp;nbsp;when LPSPI is used in half duplex because overflow interrupt is triggered and transfer fails.&lt;/P&gt;&lt;P&gt;On EAR 0.9.1 this issue will be fixed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Razvan&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Nov 2017 09:30:28 GMT</pubDate>
    <dc:creator>razva_tilimpea</dc:creator>
    <dc:date>2017-11-23T09:30:28Z</dc:date>
    <item>
      <title>S32K144 SPI half-duplex DMA</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K144-SPI-half-duplex-DMA/m-p/712516#M215</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have modified the SDK sample "lpspi_transfer_s32k144" from S32SDK_S32K14x_EAR_0.8.4 to use DMA instead of interrupts.&amp;nbsp;This involved adding a EDMA_DRV_Init() to the mainline and using&amp;nbsp;components inspector to add two new DMA channels: #1 for LPSPI0_TX&amp;nbsp;and #2 for LPSPI0_RX. These are used by the master.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This works, but eventually I just want to send from master to slave -- my eventual slave device will have no data to send back.&amp;nbsp;So I don't need or want that LPSPI0_RX DMA channel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, if I set the master's RX to "No DMA" in component inspector, the master stops sending on SPI completely. No&amp;nbsp;activity shows up on the scope on any of the SPI lines.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Similarly if I put the RX DMA back but change the line:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'courier new', courier, monospace;"&gt;LPSPI_DRV_MasterTransferBlocking(SEND, &amp;amp;masterDataSend, &amp;amp;masterDataReceive, BUFFER_SIZE, TIMEOUT);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;...to have NULL in place of &amp;amp;masterDataReceive indicating I expect to receive nothing for the master, again the SPI just stops working.&amp;nbsp;&amp;nbsp;Nothing in the driver returns any errors; the SPI lines simply do nothing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The same code works fine I switch back to using interrupts on master.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What's the trick to getting DMA just on SPI master TX to behave?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Oct 2017 17:06:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K144-SPI-half-duplex-DMA/m-p/712516#M215</guid>
      <dc:creator>pontushedman</dc:creator>
      <dc:date>2017-10-23T17:06:33Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 SPI half-duplex DMA</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K144-SPI-half-duplex-DMA/m-p/712517#M216</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, there seems to be problems with transfers &amp;gt;16 bytes (i.e. more than the SPI FIFO capacity) with both Interrupt and DMA modes when there is no Rx buffer (half duplex, i.e. NULL for receiveBuffer in the&amp;nbsp;LPSPI_DRV_MasterTransferBlocking() call). In both cases it seems to be unhandled receive overruns.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To get Interrupt driven half duplex working I had to make a change to&lt;BR /&gt;S32SDK_S32K14x_EAR_0.8.4/platform/drivers/src/lpspi/lpspi_master_driver.c .&lt;BR /&gt;In LPSPI_DRV_MasterIRQHandler(), I replaced the existing code:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: terminal, monaco, monospace;"&gt;if(LPSPI_GetStatusFlag(base,LPSPI_RX_DATA_FLAG) &amp;amp;&amp;amp; (rxCount != (uint16_t)0))&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: terminal, monaco, monospace;"&gt;{&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: terminal, monaco, monospace;"&gt;&amp;nbsp; &amp;nbsp; LPSPI_DRV_ReadRXBuffer(instance);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: terminal, monaco, monospace;"&gt;}&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;...with this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: terminal, monaco, monospace;"&gt;if (rxCount) {&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: terminal, monaco, monospace;"&gt;&amp;nbsp; &amp;nbsp; if (LPSPI_GetStatusFlag(base,LPSPI_RX_DATA_FLAG))&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: terminal, monaco, monospace;"&gt;&amp;nbsp; &amp;nbsp; {&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: terminal, monaco, monospace;"&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; LPSPI_DRV_ReadRXBuffer(instance);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: terminal, monaco, monospace;"&gt;&amp;nbsp; &amp;nbsp; }&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: terminal, monaco, monospace;"&gt; } else {&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: terminal, monaco, monospace;"&gt;&amp;nbsp; &amp;nbsp; /* No RX wanted so clear RX FIFO -- Pontus Hedman 20171031 */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: terminal, monaco, monospace;"&gt;&amp;nbsp; &amp;nbsp; LPSPI_SetFlushFifoCmd(base, false, true);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: terminal, monaco, monospace;"&gt; }&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That seemed to take care of IRQ driven code.&amp;nbsp; Meanwhile, to get DMA half duplex with &amp;gt;16 byte transfers working, I had to change LPSPI_DRV_MasterStartTransfer()&amp;nbsp; in the same file.&amp;nbsp; I replaced the existing code:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: terminal, monaco, monospace;"&gt;LPSPI_SetIntMode(base,LPSPI_RECEIVE_ERROR , true);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;...with this conditional code:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: terminal, monaco, monospace;"&gt;&lt;SPAN&gt;/* Catch Rx errors only if we actually want to receive -- Pontus Hedman 20171031 */&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: terminal, monaco, monospace;"&gt;if (receiveBuffer) {&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: terminal, monaco, monospace;"&gt;&amp;nbsp; &amp;nbsp; LPSPI_SetIntMode(base, LPSPI_RECEIVE_ERROR , true);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: terminal, monaco, monospace;"&gt; }&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In addition, in my main() of the&amp;nbsp;lpspi_transfer_s32k144 sample project I had to turn on NOSTALL so the SPI doesn't choke when transferring more than 16 bytes (FIFO capacity):&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: terminal, monaco, monospace;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: terminal, monaco, monospace;"&gt;/* Don't stall on Rx FIFO overrun on large DMAs; don't care in half duplex */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: terminal, monaco, monospace;"&gt; LPSPI_Disable(g_lpspiBase[SEND]);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: terminal, monaco, monospace;"&gt; g_lpspiBase[SEND]-&amp;gt;CFGR1 |= LPSPI_CFGR1_NOSTALL(1);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: terminal, monaco, monospace;"&gt; LPSPI_Enable(g_lpspiBase[SEND]);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't know if this is all the best or even correct solution, but it seems to work.&amp;nbsp; I'm not keen on the NOSTALL since it can cause Tx underruns, but from testing I haven't seen any.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Feedback appreciated...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Nov 2017 12:18:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K144-SPI-half-duplex-DMA/m-p/712517#M216</guid>
      <dc:creator>pontushedman</dc:creator>
      <dc:date>2017-11-02T12:18:34Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 SPI half-duplex DMA</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K144-SPI-half-duplex-DMA/m-p/712518#M217</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Nice work,&lt;/P&gt;&lt;P&gt;thanks&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Nov 2017 13:00:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K144-SPI-half-duplex-DMA/m-p/712518#M217</guid>
      <dc:creator>changfuzhao</dc:creator>
      <dc:date>2017-11-02T13:00:47Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 SPI half-duplex DMA</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K144-SPI-half-duplex-DMA/m-p/712519#M218</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your feedback.&lt;/P&gt;&lt;P&gt;We know that is a problem&amp;nbsp;when LPSPI is used in half duplex because overflow interrupt is triggered and transfer fails.&lt;/P&gt;&lt;P&gt;On EAR 0.9.1 this issue will be fixed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Razvan&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Nov 2017 09:30:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K144-SPI-half-duplex-DMA/m-p/712519#M218</guid>
      <dc:creator>razva_tilimpea</dc:creator>
      <dc:date>2017-11-23T09:30:28Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 SPI half-duplex DMA</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K144-SPI-half-duplex-DMA/m-p/712520#M219</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;good news, when it be available?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Nov 2017 00:29:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K144-SPI-half-duplex-DMA/m-p/712520#M219</guid>
      <dc:creator>changfuzhao</dc:creator>
      <dc:date>2017-11-24T00:29:03Z</dc:date>
    </item>
  </channel>
</rss>