<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 SDKのトピックS32r274 boot core</title>
    <link>https://community.nxp.com/t5/S32-SDK/S32r274-boot-core/m-p/1250464#M2129</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I created a multi-core project for S32r274 in S32 DS. When ı installed the initialization functions(clock, timer) on Z4 core, project ran correctly. When ı installed the initalization functions on Z7_1, the functions on Z4 did not work, but the functions on Z7_2 worked. Does the Z4 core have to be a boot core? What should ı do to use the Z7 core as the boot core?&lt;/P&gt;</description>
    <pubDate>Tue, 23 Mar 2021 13:20:11 GMT</pubDate>
    <dc:creator>burak_</dc:creator>
    <dc:date>2021-03-23T13:20:11Z</dc:date>
    <item>
      <title>S32r274 boot core</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32r274-boot-core/m-p/1250464#M2129</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I created a multi-core project for S32r274 in S32 DS. When ı installed the initialization functions(clock, timer) on Z4 core, project ran correctly. When ı installed the initalization functions on Z7_1, the functions on Z4 did not work, but the functions on Z7_2 worked. Does the Z4 core have to be a boot core? What should ı do to use the Z7 core as the boot core?&lt;/P&gt;</description>
      <pubDate>Tue, 23 Mar 2021 13:20:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32r274-boot-core/m-p/1250464#M2129</guid>
      <dc:creator>burak_</dc:creator>
      <dc:date>2021-03-23T13:20:11Z</dc:date>
    </item>
    <item>
      <title>Re: S32r274 boot core</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32r274-boot-core/m-p/1250611#M2130</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Z4 core is default boot core. Default multi-core project in S32DS expects this configuration. &lt;/P&gt;
&lt;P&gt;It is possible to change this by DCF record. See SSCM_UOPS register in the reference manual.&lt;/P&gt;
&lt;P&gt;Then there's file S32R274_UTest_Memory_Map_DCF_Rev11.xlsx attached inside the reference manual. Default_core (I can see the terms are not unified here) can be changed in dcl_soc_conf_1.&lt;/P&gt;
&lt;P&gt;You can take a look at this application note for more details about DCF configuration (section 4):&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12553.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12553.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Also this DCF configurator will be useful:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/S32R274-DCF-Configurator/ta-p/1102353" target="_blank"&gt;https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/S32R274-DCF-Configurator/ta-p/1102353&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;The question is if it is worth changing it. But that's up to you.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 23 Mar 2021 16:29:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32r274-boot-core/m-p/1250611#M2130</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2021-03-23T16:29:07Z</dc:date>
    </item>
  </channel>
</rss>