<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 SDKのトピックMPC5748G- UART_PAL not working</title>
    <link>https://community.nxp.com/t5/S32-SDK/MPC5748G-UART-PAL-not-working/m-p/1246985#M2116</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have changed clock to 24MHz, and trying to enable uart_pal. LINFlexD_2 is used in the given example uart_pal_mpc5748g, Where I have configured with&amp;nbsp;LINFlexD_7 instead of&amp;nbsp;LINFlexD_2.&lt;/P&gt;&lt;P&gt;But it is not working. Kindly do support.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Logan&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 17 Mar 2021 08:22:01 GMT</pubDate>
    <dc:creator>logan_r</dc:creator>
    <dc:date>2021-03-17T08:22:01Z</dc:date>
    <item>
      <title>MPC5748G- UART_PAL not working</title>
      <link>https://community.nxp.com/t5/S32-SDK/MPC5748G-UART-PAL-not-working/m-p/1246985#M2116</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have changed clock to 24MHz, and trying to enable uart_pal. LINFlexD_2 is used in the given example uart_pal_mpc5748g, Where I have configured with&amp;nbsp;LINFlexD_7 instead of&amp;nbsp;LINFlexD_2.&lt;/P&gt;&lt;P&gt;But it is not working. Kindly do support.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Logan&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Mar 2021 08:22:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/MPC5748G-UART-PAL-not-working/m-p/1246985#M2116</guid>
      <dc:creator>logan_r</dc:creator>
      <dc:date>2021-03-17T08:22:01Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G- UART_PAL not working</title>
      <link>https://community.nxp.com/t5/S32-SDK/MPC5748G-UART-PAL-not-working/m-p/1248424#M2117</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/146476"&gt;@logan_r&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;As this relates to usage of the S32 SDK, we have relocated the post to be addressed by the experts for S32 SDK.&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Thu, 18 Mar 2021 22:10:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/MPC5748G-UART-PAL-not-working/m-p/1248424#M2117</guid>
      <dc:creator>mikedoidge</dc:creator>
      <dc:date>2021-03-18T22:10:53Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G- UART_PAL not working</title>
      <link>https://community.nxp.com/t5/S32-SDK/MPC5748G-UART-PAL-not-working/m-p/1248954#M2121</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I don't have a board with 24MHz crystal, so I can't test your project directly without changes. What is not working exactly? If you use an oscilloscope, is anything send out? When you debug the code, what can you see?&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 19 Mar 2021 14:42:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/MPC5748G-UART-PAL-not-working/m-p/1248954#M2121</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2021-03-19T14:42:32Z</dc:date>
    </item>
  </channel>
</rss>