<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPSPI driver blocks when using FreeRTOS in S32 SDK</title>
    <link>https://community.nxp.com/t5/S32-SDK/LPSPI-driver-blocks-when-using-FreeRTOS/m-p/1227949#M2063</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;usually increasing size of&amp;nbsp;&lt;SPAN&gt;heap and stack of the&amp;nbsp;task would help, as mentioned e.g. in&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;&lt;A href="https://community.nxp.com/t5/S32K/S32K146-FREERTOS-LSPI-but-SPI-dones-t-work/m-p/1032623" target="_blank"&gt;https://community.nxp.com/t5/S32K/S32K146-FREERTOS-LSPI-but-SPI-dones-t-work/m-p/1032623&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Mon, 08 Feb 2021 12:02:17 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2021-02-08T12:02:17Z</dc:date>
    <item>
      <title>LPSPI driver blocks when using FreeRTOS</title>
      <link>https://community.nxp.com/t5/S32-SDK/LPSPI-driver-blocks-when-using-FreeRTOS/m-p/1227212#M2062</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm trying to use FreeRTOS in my application which involves the S32K146 with MC33664 and MC33771C.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was able to add it to my project and run it with the CAN bus enabled and it works fine. But when I try to add the LPSPI module (Both Master and Slave) for the MC33664 it blocks the execution flow. I tried re-organize interrupt priorities but with no success.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do you have any tips on how to use the LPSPI driver from the DSK with FreeRTOS?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;</description>
      <pubDate>Fri, 05 Feb 2021 15:28:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/LPSPI-driver-blocks-when-using-FreeRTOS/m-p/1227212#M2062</guid>
      <dc:creator>louis_pelletier</dc:creator>
      <dc:date>2021-02-05T15:28:56Z</dc:date>
    </item>
    <item>
      <title>Re: LPSPI driver blocks when using FreeRTOS</title>
      <link>https://community.nxp.com/t5/S32-SDK/LPSPI-driver-blocks-when-using-FreeRTOS/m-p/1227949#M2063</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;usually increasing size of&amp;nbsp;&lt;SPAN&gt;heap and stack of the&amp;nbsp;task would help, as mentioned e.g. in&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;&lt;A href="https://community.nxp.com/t5/S32K/S32K146-FREERTOS-LSPI-but-SPI-dones-t-work/m-p/1032623" target="_blank"&gt;https://community.nxp.com/t5/S32K/S32K146-FREERTOS-LSPI-but-SPI-dones-t-work/m-p/1032623&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Mon, 08 Feb 2021 12:02:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/LPSPI-driver-blocks-when-using-FreeRTOS/m-p/1227949#M2063</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2021-02-08T12:02:17Z</dc:date>
    </item>
    <item>
      <title>Re: LPSPI driver blocks when using FreeRTOS</title>
      <link>https://community.nxp.com/t5/S32-SDK/LPSPI-driver-blocks-when-using-FreeRTOS/m-p/1228809#M2064</link>
      <description>&lt;P&gt;Hello PetrS,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My apologies, I didn't find this post in my research. It did fix my problem, thank you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I also had to assign a priority to the interrupt of the LPSPI Master and Slave driver for it to work.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;</description>
      <pubDate>Tue, 09 Feb 2021 14:07:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/LPSPI-driver-blocks-when-using-FreeRTOS/m-p/1228809#M2064</guid>
      <dc:creator>louis_pelletier</dc:creator>
      <dc:date>2021-02-09T14:07:53Z</dc:date>
    </item>
  </channel>
</rss>