<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic change IP address failed in S32 SDK</title>
    <link>https://community.nxp.com/t5/S32-SDK/change-IP-address-failed/m-p/1207214#M2033</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using S32DS working on MPC5748G. And I used&amp;nbsp;LWIP instance in example.&lt;/P&gt;&lt;P&gt;Now I want to use an another IP address.&amp;nbsp;I modified it in PE, generate PE code.&amp;nbsp; Then I can ping successful but cannot&amp;nbsp;transmit data.&lt;/P&gt;&lt;P&gt;How should I do to solve the problem?&lt;/P&gt;&lt;P&gt;Thanks and best regard,&lt;/P&gt;&lt;P&gt;lixu&lt;/P&gt;</description>
    <pubDate>Wed, 06 Jan 2021 03:16:54 GMT</pubDate>
    <dc:creator>lixu</dc:creator>
    <dc:date>2021-01-06T03:16:54Z</dc:date>
    <item>
      <title>change IP address failed</title>
      <link>https://community.nxp.com/t5/S32-SDK/change-IP-address-failed/m-p/1207214#M2033</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using S32DS working on MPC5748G. And I used&amp;nbsp;LWIP instance in example.&lt;/P&gt;&lt;P&gt;Now I want to use an another IP address.&amp;nbsp;I modified it in PE, generate PE code.&amp;nbsp; Then I can ping successful but cannot&amp;nbsp;transmit data.&lt;/P&gt;&lt;P&gt;How should I do to solve the problem?&lt;/P&gt;&lt;P&gt;Thanks and best regard,&lt;/P&gt;&lt;P&gt;lixu&lt;/P&gt;</description>
      <pubDate>Wed, 06 Jan 2021 03:16:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/change-IP-address-failed/m-p/1207214#M2033</guid>
      <dc:creator>lixu</dc:creator>
      <dc:date>2021-01-06T03:16:54Z</dc:date>
    </item>
  </channel>
</rss>