<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Bug in S32 SDK 3.0.3 ProcessorExpert Component Inspector in S32 SDK</title>
    <link>https://community.nxp.com/t5/S32-SDK/Bug-in-S32-SDK-3-0-3-ProcessorExpert-Component-Inspector/m-p/1202025#M2002</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I think there is a bug in the user input validation of Processor Expert for S32 SDK 3.0.3.&lt;/P&gt;&lt;P&gt;In the eQADC component fields, there is a possibility to specify callbacks upon DMA transfer completion. Since I do not want this behavior, I specify "NULL" in these fields.&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, the validation understand NULL as the name of a callback, and it will not let me use it in more than one place: it flags an error stating a name clash.&lt;/P&gt;&lt;P&gt;I did not check but maybe the same problem exists for other ProcessorExpert components as well.&lt;/P&gt;&lt;P&gt;Is it possible to get a fix?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lucabarbiero_0-1608481766960.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/133104i50D09C6C1CB3CDA4/image-size/large?v=v2&amp;amp;px=999" role="button" title="lucabarbiero_0-1608481766960.png" alt="lucabarbiero_0-1608481766960.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sun, 20 Dec 2020 16:35:49 GMT</pubDate>
    <dc:creator>lucabarbiero</dc:creator>
    <dc:date>2020-12-20T16:35:49Z</dc:date>
    <item>
      <title>Bug in S32 SDK 3.0.3 ProcessorExpert Component Inspector</title>
      <link>https://community.nxp.com/t5/S32-SDK/Bug-in-S32-SDK-3-0-3-ProcessorExpert-Component-Inspector/m-p/1202025#M2002</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I think there is a bug in the user input validation of Processor Expert for S32 SDK 3.0.3.&lt;/P&gt;&lt;P&gt;In the eQADC component fields, there is a possibility to specify callbacks upon DMA transfer completion. Since I do not want this behavior, I specify "NULL" in these fields.&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, the validation understand NULL as the name of a callback, and it will not let me use it in more than one place: it flags an error stating a name clash.&lt;/P&gt;&lt;P&gt;I did not check but maybe the same problem exists for other ProcessorExpert components as well.&lt;/P&gt;&lt;P&gt;Is it possible to get a fix?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lucabarbiero_0-1608481766960.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/133104i50D09C6C1CB3CDA4/image-size/large?v=v2&amp;amp;px=999" role="button" title="lucabarbiero_0-1608481766960.png" alt="lucabarbiero_0-1608481766960.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 20 Dec 2020 16:35:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Bug-in-S32-SDK-3-0-3-ProcessorExpert-Component-Inspector/m-p/1202025#M2002</guid>
      <dc:creator>lucabarbiero</dc:creator>
      <dc:date>2020-12-20T16:35:49Z</dc:date>
    </item>
    <item>
      <title>Re: Bug in S32 SDK 3.0.3 ProcessorExpert Component Inspector</title>
      <link>https://community.nxp.com/t5/S32-SDK/Bug-in-S32-SDK-3-0-3-ProcessorExpert-Component-Inspector/m-p/1669212#M3158</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Could you solve the problem?&lt;/P&gt;&lt;P&gt;I am having the same issue while defining multiple I2C master configurations. I cannot define more than one callback as "NULL".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Jun 2023 10:29:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Bug-in-S32-SDK-3-0-3-ProcessorExpert-Component-Inspector/m-p/1669212#M3158</guid>
      <dc:creator>kamilla_peixoto</dc:creator>
      <dc:date>2023-06-14T10:29:43Z</dc:date>
    </item>
  </channel>
</rss>