<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32SDK LPTMR driver not linkable with IAR EW in S32 SDK</title>
    <link>https://community.nxp.com/t5/S32-SDK/S32SDK-LPTMR-driver-not-linkable-with-IAR-EW/m-p/1166661#M1931</link>
    <description>&lt;P&gt;I was able to fix that problem with the following two options:&lt;/P&gt;&lt;P&gt;Linker-&amp;gt;Library-&amp;gt;activate "Automatic runtime library selection"&lt;/P&gt;&lt;P&gt;Linker-&amp;gt;Extra Options-&amp;gt;Ensure that "--no_library_search" is &lt;U&gt;not&lt;/U&gt; present in the command line options&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;</description>
    <pubDate>Tue, 13 Oct 2020 10:05:45 GMT</pubDate>
    <dc:creator>TomLightning</dc:creator>
    <dc:date>2020-10-13T10:05:45Z</dc:date>
    <item>
      <title>S32SDK LPTMR driver not linkable with IAR EW</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32SDK-LPTMR-driver-not-linkable-with-IAR-EW/m-p/1164396#M1929</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have developed a project for the S32K142 with the S32 Design Studio. In this project I'm using certain drivers from the S32SDK. Now I'm trying to export this project into a IAR Embedded Workbench project by using the example project for the S32K142 included in the SDK as base. I added all necessary source files and the include paths for the header files as well.&lt;/P&gt;&lt;P&gt;Everytime I try to build the project I get the following errors during the linking process:&lt;/P&gt;&lt;P&gt;Error[Li005]: no definition for "__aeabi_llsl" [referenced from P:\Desktop\imported\s32k142_iar_template\Debug_FLASH\Obj\lptmr_driver.o]&lt;/P&gt;&lt;P&gt;Error[Li005]: no definition for "__aeabi_uldivmod" [referenced from P:\Desktop\imported\s32k142_iar_template\Debug_FLASH\Obj\lptmr_driver.o]&lt;/P&gt;&lt;P&gt;When I comment the following line in main.c the project is build successfully:&lt;/P&gt;&lt;P&gt;LPTMR_DRV_Init(INST_LPTMR1, &amp;amp;lpTmr1_config0, false);&lt;/P&gt;&lt;P&gt;Does anyone have an advice for me?&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;</description>
      <pubDate>Thu, 08 Oct 2020 08:52:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32SDK-LPTMR-driver-not-linkable-with-IAR-EW/m-p/1164396#M1929</guid>
      <dc:creator>TomLightning</dc:creator>
      <dc:date>2020-10-08T08:52:11Z</dc:date>
    </item>
    <item>
      <title>Re: S32SDK LPTMR driver not linkable with IAR EW</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32SDK-LPTMR-driver-not-linkable-with-IAR-EW/m-p/1166661#M1931</link>
      <description>&lt;P&gt;I was able to fix that problem with the following two options:&lt;/P&gt;&lt;P&gt;Linker-&amp;gt;Library-&amp;gt;activate "Automatic runtime library selection"&lt;/P&gt;&lt;P&gt;Linker-&amp;gt;Extra Options-&amp;gt;Ensure that "--no_library_search" is &lt;U&gt;not&lt;/U&gt; present in the command line options&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;</description>
      <pubDate>Tue, 13 Oct 2020 10:05:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32SDK-LPTMR-driver-not-linkable-with-IAR-EW/m-p/1166661#M1931</guid>
      <dc:creator>TomLightning</dc:creator>
      <dc:date>2020-10-13T10:05:45Z</dc:date>
    </item>
  </channel>
</rss>