<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 SDKのトピックRe: PIN STATE</title>
    <link>https://community.nxp.com/t5/S32-SDK/PIN-STATE/m-p/1160624#M1924</link>
    <description>&lt;P&gt;Hello Koorosh,&lt;/P&gt;
&lt;P&gt;It means that it is disconnected from all the digital peripherals in the port's MUX including GPIO.&lt;/P&gt;
&lt;P&gt;Please refer to AN5426, Hardware Design Guidelines for S32K1xx Microcontrollers.&lt;/P&gt;
&lt;P&gt;It can be found at the link below under Application Note&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/s32k-automotive-mcus/s32k1-microcontrollers-for-general-purpose:S32K?tab=Documentation_Tab" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/s32k-automotive-mcus/s32k1-microcontrollers-for-general-purpose:S32K?tab=Documentation_Tab&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Table 7. Used pins configuration&lt;/P&gt;
&lt;P&gt;Footnote 2.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 29 Sep 2020 10:58:12 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2020-09-29T10:58:12Z</dc:date>
    <item>
      <title>PIN STATE</title>
      <link>https://community.nxp.com/t5/S32-SDK/PIN-STATE/m-p/1159760#M1923</link>
      <description>&lt;P&gt;Target is S32K148:&lt;/P&gt;&lt;P&gt;In the S32k reference manual the attached spread sheet for the IO pins, the default state is marked as disabled.&lt;/P&gt;&lt;P&gt;What is meant by disabled?&lt;/P&gt;&lt;P&gt;if I don't initialize the pin in my code, what would be the current consumption for that specific pin with the default state as "Disabled"?&lt;/P&gt;&lt;P&gt;I know the best way to reduce the current consumption for the unused pin is to configure it as an input with the internal pulls enabled.&lt;/P&gt;&lt;P&gt;I'm just very curious to know what&amp;nbsp;&amp;nbsp;"disabled" state means .&lt;/P&gt;&lt;P&gt;is it totally disconnected with&amp;nbsp;CMOS structure of the pin?&amp;nbsp;is it consuming any power? what state is the&lt;/P&gt;&lt;P&gt;pin's driver gate&amp;nbsp;gate&amp;nbsp;?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Koorosh Hajiani&lt;/P&gt;</description>
      <pubDate>Sun, 27 Sep 2020 20:29:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/PIN-STATE/m-p/1159760#M1923</guid>
      <dc:creator>hajianik</dc:creator>
      <dc:date>2020-09-27T20:29:39Z</dc:date>
    </item>
    <item>
      <title>Re: PIN STATE</title>
      <link>https://community.nxp.com/t5/S32-SDK/PIN-STATE/m-p/1160624#M1924</link>
      <description>&lt;P&gt;Hello Koorosh,&lt;/P&gt;
&lt;P&gt;It means that it is disconnected from all the digital peripherals in the port's MUX including GPIO.&lt;/P&gt;
&lt;P&gt;Please refer to AN5426, Hardware Design Guidelines for S32K1xx Microcontrollers.&lt;/P&gt;
&lt;P&gt;It can be found at the link below under Application Note&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/s32k-automotive-mcus/s32k1-microcontrollers-for-general-purpose:S32K?tab=Documentation_Tab" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/s32k-automotive-mcus/s32k1-microcontrollers-for-general-purpose:S32K?tab=Documentation_Tab&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Table 7. Used pins configuration&lt;/P&gt;
&lt;P&gt;Footnote 2.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Sep 2020 10:58:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/PIN-STATE/m-p/1160624#M1924</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2020-09-29T10:58:12Z</dc:date>
    </item>
  </channel>
</rss>