<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: plain key status bit for the RAM_KEY in S32 SDK</title>
    <link>https://community.nxp.com/t5/S32-SDK/plain-key-status-bit-for-the-RAM-KEY/m-p/1151410#M1887</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;this flag is required by SHE specification. Each key has several attributes/flags which are hidden for user.&lt;/P&gt;
&lt;P&gt;Plain key flag has to be set when key is loaded as a plain RAM_KEY. The flag has to be reset when key is loaded by the secure protocol. The flag is then used to confirm if a key can be exported. Only RAM_KEY can be exported.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 10 Sep 2020 07:51:33 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2020-09-10T07:51:33Z</dc:date>
    <item>
      <title>plain key status bit for the RAM_KEY</title>
      <link>https://community.nxp.com/t5/S32-SDK/plain-key-status-bit-for-the-RAM-KEY/m-p/1151200#M1882</link>
      <description>&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using s32k144 EVB and I'm studying CSEc module.&lt;/P&gt;&lt;P&gt;In command 'CMD_LOAD_PLAION_KEY' explaination,&lt;/P&gt;&lt;P&gt;there is this phrase, "The command sets the plain key status bit for the RAM_KEY".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Where can I find plain key status bit?&lt;/P&gt;&lt;P&gt;Are there registers that show plain key status?&lt;/P&gt;</description>
      <pubDate>Thu, 10 Sep 2020 01:56:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/plain-key-status-bit-for-the-RAM-KEY/m-p/1151200#M1882</guid>
      <dc:creator>skseofh</dc:creator>
      <dc:date>2020-09-10T01:56:02Z</dc:date>
    </item>
    <item>
      <title>Re: plain key status bit for the RAM_KEY</title>
      <link>https://community.nxp.com/t5/S32-SDK/plain-key-status-bit-for-the-RAM-KEY/m-p/1151202#M1883</link>
      <description>&lt;P&gt;S32K-RM(page 899)&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="skseofh_0-1599702974279.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/124787i15789D3DB8167141/image-size/medium?v=v2&amp;amp;px=400" role="button" title="skseofh_0-1599702974279.png" alt="skseofh_0-1599702974279.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Sep 2020 01:57:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/plain-key-status-bit-for-the-RAM-KEY/m-p/1151202#M1883</guid>
      <dc:creator>skseofh</dc:creator>
      <dc:date>2020-09-10T01:57:09Z</dc:date>
    </item>
    <item>
      <title>Re: plain key status bit for the RAM_KEY</title>
      <link>https://community.nxp.com/t5/S32-SDK/plain-key-status-bit-for-the-RAM-KEY/m-p/1151410#M1887</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;this flag is required by SHE specification. Each key has several attributes/flags which are hidden for user.&lt;/P&gt;
&lt;P&gt;Plain key flag has to be set when key is loaded as a plain RAM_KEY. The flag has to be reset when key is loaded by the secure protocol. The flag is then used to confirm if a key can be exported. Only RAM_KEY can be exported.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Sep 2020 07:51:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/plain-key-status-bit-for-the-RAM-KEY/m-p/1151410#M1887</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2020-09-10T07:51:33Z</dc:date>
    </item>
  </channel>
</rss>