<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic s32k oc_pal question in S32 SDK</title>
    <link>https://community.nxp.com/t5/S32-SDK/s32k-oc-pal-question/m-p/1149299#M1861</link>
    <description>&lt;P&gt;Hello. I am a newbie who started using S32K for the first time.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;While using the OC_pal function, there is something strange, so I write.&lt;/P&gt;&lt;P&gt;I want the timer interrupt to happen per second. So, I set Disable Output as shown in the picture below.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="캡처.PNG" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/124443i2465CD69BBB66716/image-size/large?v=v2&amp;amp;px=999" role="button" title="캡처.PNG" alt="캡처.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;However, I am having a problem with DEV_ASSERT in the OC_InitFtm function.&lt;/P&gt;&lt;P&gt;If the function is OC_DISABLE_OUTPUT, it falls into an infinite loop.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="캡처2.PNG" style="width: 580px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/124444i5FA9D11DE692E8E3/image-size/large?v=v2&amp;amp;px=999" role="button" title="캡처2.PNG" alt="캡처2.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Is there a problem with the SDK? Or maybe I shouldn't use the DISABLE_OUTPUT setting?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sun, 06 Sep 2020 14:35:27 GMT</pubDate>
    <dc:creator>hyunyong1125</dc:creator>
    <dc:date>2020-09-06T14:35:27Z</dc:date>
    <item>
      <title>s32k oc_pal question</title>
      <link>https://community.nxp.com/t5/S32-SDK/s32k-oc-pal-question/m-p/1149299#M1861</link>
      <description>&lt;P&gt;Hello. I am a newbie who started using S32K for the first time.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;While using the OC_pal function, there is something strange, so I write.&lt;/P&gt;&lt;P&gt;I want the timer interrupt to happen per second. So, I set Disable Output as shown in the picture below.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="캡처.PNG" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/124443i2465CD69BBB66716/image-size/large?v=v2&amp;amp;px=999" role="button" title="캡처.PNG" alt="캡처.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;However, I am having a problem with DEV_ASSERT in the OC_InitFtm function.&lt;/P&gt;&lt;P&gt;If the function is OC_DISABLE_OUTPUT, it falls into an infinite loop.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="캡처2.PNG" style="width: 580px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/124444i5FA9D11DE692E8E3/image-size/large?v=v2&amp;amp;px=999" role="button" title="캡처2.PNG" alt="캡처2.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Is there a problem with the SDK? Or maybe I shouldn't use the DISABLE_OUTPUT setting?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 06 Sep 2020 14:35:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/s32k-oc-pal-question/m-p/1149299#M1861</guid>
      <dc:creator>hyunyong1125</dc:creator>
      <dc:date>2020-09-06T14:35:27Z</dc:date>
    </item>
    <item>
      <title>Re: s32k oc_pal question</title>
      <link>https://community.nxp.com/t5/S32-SDK/s32k-oc-pal-question/m-p/1149929#M1869</link>
      <description>&lt;P&gt;Hi&amp;nbsp;hyunyong1125,&lt;/P&gt;
&lt;P&gt;There are only three types of Output Compare mode. Disable Output seems not included in Output Compare mode.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Table 47-5. Channel Modes Selection.png" style="width: 905px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/124553i6B80FCA5F588D29D/image-size/large?v=v2&amp;amp;px=999" role="button" title="Table 47-5. Channel Modes Selection.png" alt="Table 47-5. Channel Modes Selection.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;If you don't need pin output, LPTMR and LPIT module is more suitable than FTM.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="periodic_interrupt.png" style="width: 816px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/124554i5F63CB39F1D72EF2/image-size/large?v=v2&amp;amp;px=999" role="button" title="periodic_interrupt.png" alt="periodic_interrupt.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;/P&gt;
&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 08 Sep 2020 02:10:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/s32k-oc-pal-question/m-p/1149929#M1869</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2020-09-08T02:10:33Z</dc:date>
    </item>
    <item>
      <title>Re: s32k oc_pal question</title>
      <link>https://community.nxp.com/t5/S32-SDK/s32k-oc-pal-question/m-p/1150367#M1873</link>
      <description>&lt;P&gt;Hi Robin_Shen&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you so much for your clear answer.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Additional Question.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1. There are only 3 functions of output compare. Why are there 4 menus?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;2. &lt;SPAN&gt;Do you have any documentation comparing the functions of FTM, LPIT, and LPTMR?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 08 Sep 2020 12:39:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/s32k-oc-pal-question/m-p/1150367#M1873</guid>
      <dc:creator>hyunyong1125</dc:creator>
      <dc:date>2020-09-08T12:39:58Z</dc:date>
    </item>
    <item>
      <title>Re: s32k oc_pal question</title>
      <link>https://community.nxp.com/t5/S32-SDK/s32k-oc-pal-question/m-p/1151891#M1893</link>
      <description>&lt;P&gt;1. There are only 3 functions of output compare. Why are there 4 menus?&lt;BR /&gt;A1: I will report it to internal team.&lt;/P&gt;
&lt;P&gt;2. Do you have any documentation comparing the functions of FTM, LPIT, and LPTMR?&lt;BR /&gt;A2: I did not find such documentation, maybe you have to read the "Introduction" of each module in &lt;A id="recommendedDocsLink_1" href="https://www.nxp.com/webapp/Download?colCode=S32K1XXRM" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;S32K1xx MCU Family - Reference Manual&lt;/STRONG&gt;&lt;/A&gt; to compare the difference.&lt;/P&gt;</description>
      <pubDate>Fri, 11 Sep 2020 03:11:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/s32k-oc-pal-question/m-p/1151891#M1893</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2020-09-11T03:11:53Z</dc:date>
    </item>
  </channel>
</rss>