<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 SDKのトピックRe: MPC5777C DSPI Master transmit using DMA</title>
    <link>https://community.nxp.com/t5/S32-SDK/MPC5777C-DSPI-Master-transmit-using-DMA/m-p/1097660#M1813</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lukas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I agree with the&amp;nbsp;additional DMA channel should be linked to the channel which is not used yet. But&amp;nbsp;when I used DMA channel 35 and configured the &lt;STRONG&gt;ProcessorExpert&lt;/STRONG&gt;&amp;nbsp;by adding it to the Channels list in &lt;STRONG&gt;dmaController&lt;/STRONG&gt; and selecting channel 35 for TX additional DMA channel in &lt;STRONG&gt;dspi0&lt;/STRONG&gt;, the &lt;STRONG&gt;ProcessorExpert&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;reported the error for&amp;nbsp;&lt;STRONG&gt;dmaController &lt;/STRONG&gt;so that&lt;STRONG&gt;&amp;nbsp;&lt;/STRONG&gt;can't generate code successfully.&lt;STRONG&gt;&amp;nbsp;&lt;/STRONG&gt;A&lt;/SPAN&gt;s shown in the following figures.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22724i425C3DB698248F1F/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22741i7DE4795A2F644A98/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22794iA65BB36724EB0454/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To generate code successfully, I had to select the channel 32 as TX additional DMA channel, and then changed&amp;nbsp;it to channel 35 manually in the code to ensure that the additional DMA channel can successfully transfer the master command to TX PUSHR. I have confirmed this operation is OK.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22469i18667B5ADF86620F/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So is it an issue for SDK or there are other operations to configure this additional channel?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Aug 2020 05:17:18 GMT</pubDate>
    <dc:creator>Dong_Luo</dc:creator>
    <dc:date>2020-08-20T05:17:18Z</dc:date>
    <item>
      <title>MPC5777C DSPI Master transmit using DMA</title>
      <link>https://community.nxp.com/t5/S32-SDK/MPC5777C-DSPI-Master-transmit-using-DMA/m-p/1097657#M1810</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working on the DSPI master transmit using DMA which based on SDK.&amp;nbsp; I just used DSPI0 loopback mode that connects SOUT to SIN,&amp;nbsp; and no idea about the TX additional DMA channel.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/115116i59C94949B49C7140/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I checked the SDK user manual that explains this channel is used to push commands in the corresponding FIFO, but as for the specify DMA channel, which channel should I choose?&amp;nbsp;I have confirmed that channel 33 is not working. And when I choose the other channel such as channel 35, it will conflict with ESCI_1_RX request.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/115117i61618E06A595CED6/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Aug 2020 07:08:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/MPC5777C-DSPI-Master-transmit-using-DMA/m-p/1097657#M1810</guid>
      <dc:creator>Dong_Luo</dc:creator>
      <dc:date>2020-08-17T07:08:19Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5777C DSPI Master transmit using DMA</title>
      <link>https://community.nxp.com/t5/S32-SDK/MPC5777C-DSPI-Master-transmit-using-DMA/m-p/1097658#M1811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think it might be ProcessorExpert&amp;nbsp;issues. It&amp;nbsp;is working when I modified the txAdditionalDMAChannel manually before call&amp;nbsp;DSPI_MasterInit.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/115166iA8EB3A7E7B63F4FE/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Aug 2020 10:48:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/MPC5777C-DSPI-Master-transmit-using-DMA/m-p/1097658#M1811</guid>
      <dc:creator>Dong_Luo</dc:creator>
      <dc:date>2020-08-17T10:48:41Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5777C DSPI Master transmit using DMA</title>
      <link>https://community.nxp.com/t5/S32-SDK/MPC5777C-DSPI-Master-transmit-using-DMA/m-p/1097659#M1812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dong,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;there's no DMA MUX on this device, the peripheral requests are hardwired to given DMA channels. That means you must use channels 32 and 33 for DSPI TX and RX:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/115196i0BF029DBB7B912FC/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt; &lt;/P&gt;&lt;P&gt;The additional DMA channel does not use hardware request from DSPI peripheral. Linking is used from channel 32. The "Request" field obviously shows corresponding hardware request regardless of this configuration.&lt;/P&gt;&lt;P&gt;It should be possible to use any DMA channel which is not used yet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Aug 2020 10:07:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/MPC5777C-DSPI-Master-transmit-using-DMA/m-p/1097659#M1812</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2020-08-18T10:07:25Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5777C DSPI Master transmit using DMA</title>
      <link>https://community.nxp.com/t5/S32-SDK/MPC5777C-DSPI-Master-transmit-using-DMA/m-p/1097660#M1813</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lukas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I agree with the&amp;nbsp;additional DMA channel should be linked to the channel which is not used yet. But&amp;nbsp;when I used DMA channel 35 and configured the &lt;STRONG&gt;ProcessorExpert&lt;/STRONG&gt;&amp;nbsp;by adding it to the Channels list in &lt;STRONG&gt;dmaController&lt;/STRONG&gt; and selecting channel 35 for TX additional DMA channel in &lt;STRONG&gt;dspi0&lt;/STRONG&gt;, the &lt;STRONG&gt;ProcessorExpert&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;reported the error for&amp;nbsp;&lt;STRONG&gt;dmaController &lt;/STRONG&gt;so that&lt;STRONG&gt;&amp;nbsp;&lt;/STRONG&gt;can't generate code successfully.&lt;STRONG&gt;&amp;nbsp;&lt;/STRONG&gt;A&lt;/SPAN&gt;s shown in the following figures.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22724i425C3DB698248F1F/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22741i7DE4795A2F644A98/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22794iA65BB36724EB0454/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To generate code successfully, I had to select the channel 32 as TX additional DMA channel, and then changed&amp;nbsp;it to channel 35 manually in the code to ensure that the additional DMA channel can successfully transfer the master command to TX PUSHR. I have confirmed this operation is OK.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22469i18667B5ADF86620F/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So is it an issue for SDK or there are other operations to configure this additional channel?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Aug 2020 05:17:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/MPC5777C-DSPI-Master-transmit-using-DMA/m-p/1097660#M1813</guid>
      <dc:creator>Dong_Luo</dc:creator>
      <dc:date>2020-08-20T05:17:18Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5777C DSPI Master transmit using DMA</title>
      <link>https://community.nxp.com/t5/S32-SDK/MPC5777C-DSPI-Master-transmit-using-DMA/m-p/1097661#M1814</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dong,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you share the error message?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Razvan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Aug 2020 07:56:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/MPC5777C-DSPI-Master-transmit-using-DMA/m-p/1097661#M1814</guid>
      <dc:creator>razva_tilimpea</dc:creator>
      <dc:date>2020-08-20T07:56:53Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5777C DSPI Master transmit using DMA</title>
      <link>https://community.nxp.com/t5/S32-SDK/MPC5777C-DSPI-Master-transmit-using-DMA/m-p/1097662#M1815</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Razvan-nicolae,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here are some screen captures for error message.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/70546i2715E8550D800C70/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/70593iE2CC0B17D0764F60/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Aug 2020 10:08:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/MPC5777C-DSPI-Master-transmit-using-DMA/m-p/1097662#M1815</guid>
      <dc:creator>Dong_Luo</dc:creator>
      <dc:date>2020-08-20T10:08:33Z</dc:date>
    </item>
  </channel>
</rss>