<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 SDKのトピックS32K144 FreeRTOS  interrupt function conflict</title>
    <link>https://community.nxp.com/t5/S32-SDK/S32K144-FreeRTOS-interrupt-function-conflict/m-p/1086051#M1770</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Under FreeRTOS, as long as when you start the interrupt function of the callback function&amp;nbsp; is&amp;nbsp; not normal, it run where the function DefaultISR. It is normal when run&amp;nbsp;not use FreeRTOS, there is a&amp;nbsp; conflict between the original interrupt and FreeRTOS, how can I solve it？Thanks!&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/115510iBE98877797CEA664/image-size/large?v=v2&amp;amp;px=999" title="搜狗截图20200710171737.png" alt="搜狗截图20200710171737.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 Jul 2020 09:23:02 GMT</pubDate>
    <dc:creator>gongchangyu</dc:creator>
    <dc:date>2020-07-10T09:23:02Z</dc:date>
    <item>
      <title>S32K144 FreeRTOS  interrupt function conflict</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K144-FreeRTOS-interrupt-function-conflict/m-p/1086051#M1770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Under FreeRTOS, as long as when you start the interrupt function of the callback function&amp;nbsp; is&amp;nbsp; not normal, it run where the function DefaultISR. It is normal when run&amp;nbsp;not use FreeRTOS, there is a&amp;nbsp; conflict between the original interrupt and FreeRTOS, how can I solve it？Thanks!&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/115510iBE98877797CEA664/image-size/large?v=v2&amp;amp;px=999" title="搜狗截图20200710171737.png" alt="搜狗截图20200710171737.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jul 2020 09:23:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K144-FreeRTOS-interrupt-function-conflict/m-p/1086051#M1770</guid>
      <dc:creator>gongchangyu</dc:creator>
      <dc:date>2020-07-10T09:23:02Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 FreeRTOS  interrupt function conflict</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K144-FreeRTOS-interrupt-function-conflict/m-p/1086052#M1771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which drivers are used in your application?&lt;/P&gt;&lt;P&gt;How do you initialize them? Before starting scheduler?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Razvan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jul 2020 06:54:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K144-FreeRTOS-interrupt-function-conflict/m-p/1086052#M1771</guid>
      <dc:creator>razva_tilimpea</dc:creator>
      <dc:date>2020-07-14T06:54:19Z</dc:date>
    </item>
  </channel>
</rss>