<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 SDKのトピックEmpty signal spaces being set on LIN Stack</title>
    <link>https://community.nxp.com/t5/S32-SDK/Empty-signal-spaces-being-set-on-LIN-Stack/m-p/1061027#M1678</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question related to the autogenerated code after setting up my .ldf file using the SDK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I finished setting everything up, I noticed that the array that keeps track of the LIN signal values is initialized according to the configuration. However, bytes which belong to a message but do not have a signal assigned (empty message bytes) or bits within a byte that also don't have a signal assigned are given a "set" default value. For example, empty bytes are given 0xFF as default values and empty bits are set to be 1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="StackBitsQuestion.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22863iF3A5D7494E2E6443/image-size/large?v=v2&amp;amp;px=999" role="button" title="StackBitsQuestion.PNG" alt="StackBitsQuestion.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In the screenshot, signals values within the blue circle are examples of unwanted set bits or empty&amp;nbsp;positions&amp;nbsp;set as 0xFF&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a configuration that I could change to make this reset instead of set? (zeroes instead of ones) Or do I have to manually set those values?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Apr 2020 14:15:27 GMT</pubDate>
    <dc:creator>joseponc</dc:creator>
    <dc:date>2020-04-21T14:15:27Z</dc:date>
    <item>
      <title>Empty signal spaces being set on LIN Stack</title>
      <link>https://community.nxp.com/t5/S32-SDK/Empty-signal-spaces-being-set-on-LIN-Stack/m-p/1061027#M1678</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question related to the autogenerated code after setting up my .ldf file using the SDK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I finished setting everything up, I noticed that the array that keeps track of the LIN signal values is initialized according to the configuration. However, bytes which belong to a message but do not have a signal assigned (empty message bytes) or bits within a byte that also don't have a signal assigned are given a "set" default value. For example, empty bytes are given 0xFF as default values and empty bits are set to be 1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="StackBitsQuestion.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22863iF3A5D7494E2E6443/image-size/large?v=v2&amp;amp;px=999" role="button" title="StackBitsQuestion.PNG" alt="StackBitsQuestion.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In the screenshot, signals values within the blue circle are examples of unwanted set bits or empty&amp;nbsp;positions&amp;nbsp;set as 0xFF&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a configuration that I could change to make this reset instead of set? (zeroes instead of ones) Or do I have to manually set those values?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Apr 2020 14:15:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Empty-signal-spaces-being-set-on-LIN-Stack/m-p/1061027#M1678</guid>
      <dc:creator>joseponc</dc:creator>
      <dc:date>2020-04-21T14:15:27Z</dc:date>
    </item>
    <item>
      <title>Re: Empty signal spaces being set on LIN Stack</title>
      <link>https://community.nxp.com/t5/S32-SDK/Empty-signal-spaces-being-set-on-LIN-Stack/m-p/1061028#M1679</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, the SDK Linstack doesn't support the feature which you mention. But because these data do not belong any signal,&amp;nbsp;I think that we don't need to care about it. So&amp;nbsp;you will need to do it manually.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Hung&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Apr 2020 08:47:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Empty-signal-spaces-being-set-on-LIN-Stack/m-p/1061028#M1679</guid>
      <dc:creator>hungnguyenphi</dc:creator>
      <dc:date>2020-04-23T08:47:06Z</dc:date>
    </item>
  </channel>
</rss>