<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 SDKのトピックS32G Linux kernel panic on pfeng module</title>
    <link>https://community.nxp.com/t5/S32-SDK/S32G-Linux-kernel-panic-on-pfeng-module/m-p/1040955#M1590</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I built Linux image from bsp24.0, fsl-image-base, the ddr settings were generated from S32DS tools. I saw Linux kernel panic during boot up late stage. It did not happen every time, hit this every 10-20 times power cycles. U-boot, dtb, kernel and rootfs are flashed into emmc. Please advise. The full log file is also attached.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[ 4.326893] Unable to handle kernel NULL pointer dereference at virtual address 0000000000000060&lt;BR /&gt;[ 4.326895] Mem abort info:&lt;BR /&gt;[ 4.326898] ESR = 0x96000005&lt;BR /&gt;[ 4.326902] Exception class = DABT (current EL), IL = 32 bits&lt;BR /&gt;[ 4.326905] SET = 0, FnV = 0&lt;BR /&gt;[ 4.326907] EA = 0, S1PTW = 0&lt;BR /&gt;[ 4.326909] Data abort info:&lt;BR /&gt;[ 4.326912] ISV = 0, ISS = 0x00000005&lt;BR /&gt;[ 4.326914] CM = 0, WnR = 0&lt;BR /&gt;[ 4.326923] user pgtable: 4k pages, 39-bit VAs, pgdp = 00000000d3bfd33d&lt;BR /&gt;[ 4.326926] [0000000000000060] pgd=0000000000000000, pud=0000000000000000&lt;BR /&gt;[ 4.326937] Internal error: Oops: 96000005 [#1] PREEMPT SMP&lt;BR /&gt;[ 4.326945] Modules linked in: nxp pfeng(O)&lt;BR /&gt;[ 4.326958] Process rngd (pid: 873, stack limit = 0x00000000f0b17534)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Xiaodong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Jun 2020 18:49:45 GMT</pubDate>
    <dc:creator>xhu</dc:creator>
    <dc:date>2020-06-12T18:49:45Z</dc:date>
    <item>
      <title>S32G Linux kernel panic on pfeng module</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32G-Linux-kernel-panic-on-pfeng-module/m-p/1040955#M1590</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I built Linux image from bsp24.0, fsl-image-base, the ddr settings were generated from S32DS tools. I saw Linux kernel panic during boot up late stage. It did not happen every time, hit this every 10-20 times power cycles. U-boot, dtb, kernel and rootfs are flashed into emmc. Please advise. The full log file is also attached.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[ 4.326893] Unable to handle kernel NULL pointer dereference at virtual address 0000000000000060&lt;BR /&gt;[ 4.326895] Mem abort info:&lt;BR /&gt;[ 4.326898] ESR = 0x96000005&lt;BR /&gt;[ 4.326902] Exception class = DABT (current EL), IL = 32 bits&lt;BR /&gt;[ 4.326905] SET = 0, FnV = 0&lt;BR /&gt;[ 4.326907] EA = 0, S1PTW = 0&lt;BR /&gt;[ 4.326909] Data abort info:&lt;BR /&gt;[ 4.326912] ISV = 0, ISS = 0x00000005&lt;BR /&gt;[ 4.326914] CM = 0, WnR = 0&lt;BR /&gt;[ 4.326923] user pgtable: 4k pages, 39-bit VAs, pgdp = 00000000d3bfd33d&lt;BR /&gt;[ 4.326926] [0000000000000060] pgd=0000000000000000, pud=0000000000000000&lt;BR /&gt;[ 4.326937] Internal error: Oops: 96000005 [#1] PREEMPT SMP&lt;BR /&gt;[ 4.326945] Modules linked in: nxp pfeng(O)&lt;BR /&gt;[ 4.326958] Process rngd (pid: 873, stack limit = 0x00000000f0b17534)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Xiaodong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jun 2020 18:49:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32G-Linux-kernel-panic-on-pfeng-module/m-p/1040955#M1590</guid>
      <dc:creator>xhu</dc:creator>
      <dc:date>2020-06-12T18:49:45Z</dc:date>
    </item>
    <item>
      <title>Re: S32G Linux kernel panic on pfeng module</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32G-Linux-kernel-panic-on-pfeng-module/m-p/1040956#M1591</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Based on this information, it is not possible to establish the root cause of the&lt;BR /&gt;problem. Kernel panic is a normal reaction to broken pointers, the fact that &lt;BR /&gt;it happens from time to time points towards possible&amp;nbsp; memory decay.&lt;BR /&gt;The suggestions therefore are, test the system memory and debug your kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Platon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jul 2020 05:49:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32G-Linux-kernel-panic-on-pfeng-module/m-p/1040956#M1591</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2020-07-02T05:49:04Z</dc:date>
    </item>
  </channel>
</rss>