<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 SDKのトピックRe: S32K146 Flash read</title>
    <link>https://community.nxp.com/t5/S32-SDK/S32K146-Flash-read/m-p/1034908#M1579</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot. I could read D-Flash by simply accessing it through a pointer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adria&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Nov 2019 17:11:28 GMT</pubDate>
    <dc:creator>adria</dc:creator>
    <dc:date>2019-11-27T17:11:28Z</dc:date>
    <item>
      <title>S32K146 Flash read</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K146-Flash-read/m-p/1034906#M1577</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the&amp;nbsp;SDK RTM 3.0.0.&lt;/P&gt;&lt;P&gt;After writing into Flash (no matter whether it is P or D without the Eeprom functionality enabled) and reseting the MCU, I would like to read&amp;nbsp;the written&amp;nbsp;data,&amp;nbsp;which&amp;nbsp;API should I use to do so?&amp;nbsp;I have taken a look at&amp;nbsp;FLASH_DRV_ReadResource() but&amp;nbsp;I am not sure if it is the correct one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adria&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Nov 2019 00:54:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K146-Flash-read/m-p/1034906#M1577</guid>
      <dc:creator>adria</dc:creator>
      <dc:date>2019-11-26T00:54:08Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 Flash read</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K146-Flash-read/m-p/1034907#M1578</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adria,&lt;/P&gt;&lt;P&gt;The SDK Flash Driver doesn't have any function for reading.&lt;/P&gt;&lt;P&gt;But knowing the address of the data, you can simply read it with a pointer.&lt;/P&gt;&lt;P&gt;The&amp;nbsp;FLASH_DRV_ReadResource() function is executing READ_RESOURCE flash command as you can see in the flash_driver.c file. The S32K1xx series doesn't&amp;nbsp;have such a flash command though.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Nov 2019 13:26:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K146-Flash-read/m-p/1034907#M1578</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2019-11-27T13:26:44Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 Flash read</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32K146-Flash-read/m-p/1034908#M1579</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot. I could read D-Flash by simply accessing it through a pointer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adria&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Nov 2019 17:11:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32K146-Flash-read/m-p/1034908#M1579</guid>
      <dc:creator>adria</dc:creator>
      <dc:date>2019-11-27T17:11:28Z</dc:date>
    </item>
  </channel>
</rss>