<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 SDKのトピックRe: S32 Design Studio for Power Architecture have some bug.</title>
    <link>https://community.nxp.com/t5/S32-SDK/S32-Design-Studio-for-Power-Architecture-have-some-bug/m-p/1032485#M1548</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can you provide what version of SDK&amp;nbsp;and compiler do you use ?!&lt;/P&gt;&lt;P&gt;The buss off appear on CAN1 or both CAN1 and CAN0 when you disconnect the CAN1 ?!&lt;/P&gt;&lt;P&gt;All the CAN interface are connected to the same CAN bus ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Feb 2020 09:28:04 GMT</pubDate>
    <dc:creator>alexandrunan</dc:creator>
    <dc:date>2020-02-19T09:28:04Z</dc:date>
    <item>
      <title>S32 Design Studio for Power Architecture have some bug.</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32-Design-Studio-for-Power-Architecture-have-some-bug/m-p/1032484#M1547</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Currently, I use S32 design studio to development MPC5746B.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But, I have some trouble.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To explain my current development environment(Processor Expert).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Add Can_pal (Ch0 ~ Ch2)&lt;/P&gt;&lt;P&gt;2. Can0 ~ Can1 : CAN (High speed)&lt;/P&gt;&lt;P&gt;3. Can2 : CAN FD&lt;/P&gt;&lt;P&gt;4. CAN Ch0 ~ 2 enable Tx, Rx, Bus off Interrupt.&lt;/P&gt;&lt;P&gt;5. CAN0 - Rx : mb 0 ~ 31,&amp;nbsp; Tx : mb 32 ~ 64 (Tx, Rx bus load&amp;nbsp;between 5% and 15%)&lt;/P&gt;&lt;P&gt;6.&amp;nbsp;&lt;SPAN&gt;CAN1 - Rx : mb 0 ~ 31,&amp;nbsp; Tx : mb 32 ~ 64 (Tx, Rx bus load&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;between 1% and 3%)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;7.&amp;nbsp;&lt;SPAN&gt;CAN2 - Rx : mb 0 ~ 31,&amp;nbsp; Tx : mb 32 ~ 64 (Tx, Rx bus load&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;between 80% and 90%)&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;When i used Can0 &amp;amp; Can2 , I can communicate without problems.(Include Tx, Rx, BusOff Interrupt)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BUT&lt;/P&gt;&lt;P&gt;When&amp;nbsp;&lt;SPAN&gt;i used Can0 &amp;amp; Can1 &amp;amp; Can2, I have big problems!!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;if CAN1 Line disconnected with CAN Interface, CAN1's &amp;amp; CAN0's Busoff interrupt occurs (Confirmed via T32.).&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;So CAN0 also cannot communicate.(CAN0 &amp;amp; CAN1 BusOff state)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't&amp;nbsp;understood whether the state of CAN1 affects CAN0.&lt;/P&gt;&lt;P&gt;Why? ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have to solve this problem to keep my project schedule.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Feb 2020 01:29:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32-Design-Studio-for-Power-Architecture-have-some-bug/m-p/1032484#M1547</guid>
      <dc:creator>limsunghyun</dc:creator>
      <dc:date>2020-02-17T01:29:28Z</dc:date>
    </item>
    <item>
      <title>Re: S32 Design Studio for Power Architecture have some bug.</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32-Design-Studio-for-Power-Architecture-have-some-bug/m-p/1032485#M1548</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can you provide what version of SDK&amp;nbsp;and compiler do you use ?!&lt;/P&gt;&lt;P&gt;The buss off appear on CAN1 or both CAN1 and CAN0 when you disconnect the CAN1 ?!&lt;/P&gt;&lt;P&gt;All the CAN interface are connected to the same CAN bus ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Feb 2020 09:28:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32-Design-Studio-for-Power-Architecture-have-some-bug/m-p/1032485#M1548</guid>
      <dc:creator>alexandrunan</dc:creator>
      <dc:date>2020-02-19T09:28:04Z</dc:date>
    </item>
    <item>
      <title>Re: S32 Design Studio for Power Architecture have some bug.</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32-Design-Studio-for-Power-Architecture-have-some-bug/m-p/1032486#M1549</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. S32 Design Studio for Power Architecture v2.1&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; S32_SDK_S32PA_RTM_3.0.0 (GNU C)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Yes,&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;The bus off appear on CAN1 or both CAN1 and CAN0 when i disconnect the CAN1.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;3.&amp;nbsp;Each CAN channel uses a different bus.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Feb 2020 00:07:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32-Design-Studio-for-Power-Architecture-have-some-bug/m-p/1032486#M1549</guid>
      <dc:creator>limsunghyun</dc:creator>
      <dc:date>2020-02-20T00:07:45Z</dc:date>
    </item>
  </channel>
</rss>