<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 SDKのトピックS32v232 with Linux Kernel 4.19.31</title>
    <link>https://community.nxp.com/t5/S32-SDK/S32v232-with-Linux-Kernel-4-19-31/m-p/1023834#M1491</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can anyone advice me with this error code?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unable to handle kernel paging request at virtual address &lt;STRONG&gt;ffffffff800005c0&lt;/STRONG&gt;&lt;BR /&gt; Mem abort info:&lt;BR /&gt; ESR = 0x96000145&lt;BR /&gt; Exception class = DABT (current EL), IL = 32 bits&lt;BR /&gt; SET = 0, FnV = 0&lt;BR /&gt; EA = 0, S1PTW = 0&lt;BR /&gt; Data abort info:&lt;BR /&gt; ISV = 0, ISS = 0x00000145&lt;BR /&gt; CM = 1, WnR = 1&lt;BR /&gt; swapper pgtable: 4k pages, 39-bit VAs, pgdp = 00000000b9ddca07&lt;BR /&gt; [ffffffff800005c0] pgd=0000000000000000, pud=0000000000000000&lt;BR /&gt; Internal error: Oops: 96000145 [#1] SMP&lt;BR /&gt; Modules linked in: xxxxx(O)&lt;BR /&gt; CPU: 0 PID: 0 Comm: swapper/0 Tainted: G O 4.19.31-xxxx&lt;BR /&gt; Hardware name:&amp;nbsp;xxxxx based on Freescale S32V234 (DT)&lt;BR /&gt; pstate: 00000085 (nzcv daIf -PAN -UAO)&lt;BR /&gt; pc : &lt;STRONG&gt;__dma_inv_area+0x28/0x58&lt;/STRONG&gt;&lt;BR /&gt; lr : __swiotlb_sync_single_for_cpu+0x4c/0x70&lt;BR /&gt; sp : ffffff8008003cc0&lt;BR /&gt; x29: ffffff8008003cc0 x28: ffffff80006b5000 &lt;BR /&gt; x27: ffffffc03c420800 x26: ffffff80006b5000 &lt;BR /&gt; x25: ffffffc03c420800 x24: 000000000000003c &lt;BR /&gt; x23: ffffffc03c4a7a00 x22: ffffffc03c420000 &lt;BR /&gt; x21: 00000000000005f3 x20: 0000000000000000 &lt;BR /&gt; x19: ffffffc03dd6a0a8 x18: ffffffffffffffff &lt;BR /&gt; x17: 0000000000000001 x16: 0000000000000007 &lt;BR /&gt; x15: ffffff80088c8588 x14: ffffff808892189f &lt;BR /&gt; x13: ffffff80089218ad x12: 0000000000000000 &lt;BR /&gt; x11: ffffff80083c1090 x10: 0000000005f5e0ff &lt;BR /&gt; x9 : 00000000ffffffd0 x8 : 323033203a747075 &lt;BR /&gt; x7 : ffffff80088c85b8 x6 : 00000000000003ee &lt;BR /&gt; x5 : 0000000000000001 x4 : ffffffff80000000 &lt;BR /&gt; x3 : 000000000000003f x2 : 0000000000000040 &lt;BR /&gt; x1 : ffffffff800005c0 x0 : ffffffff80000000 &lt;BR /&gt; Process swapper/0 (pid: 0, stack limit = 0x00000000057e45cf)&lt;BR /&gt; Call trace:&lt;BR /&gt; __dma_inv_area+0x28/0x58&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Code: d1000443 ea03003f 8a230021 54000040 (d50b7e21) &lt;BR /&gt; ---[ end trace 263bcb19fc625165 ]---&lt;BR /&gt; Kernel panic - not syncing: Fatal exception in interrupt&lt;BR /&gt; SMP: stopping secondary CPUs&lt;BR /&gt; Kernel Offset: disabled&lt;BR /&gt; CPU features: 0x0,20802004&lt;BR /&gt; Memory Limit: none&lt;BR /&gt; ---[ end Kernel panic - not syncing: Fatal exception in interrupt ]---&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Nov 2019 13:58:23 GMT</pubDate>
    <dc:creator>larry_chur</dc:creator>
    <dc:date>2019-11-21T13:58:23Z</dc:date>
    <item>
      <title>S32v232 with Linux Kernel 4.19.31</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32v232-with-Linux-Kernel-4-19-31/m-p/1023834#M1491</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can anyone advice me with this error code?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unable to handle kernel paging request at virtual address &lt;STRONG&gt;ffffffff800005c0&lt;/STRONG&gt;&lt;BR /&gt; Mem abort info:&lt;BR /&gt; ESR = 0x96000145&lt;BR /&gt; Exception class = DABT (current EL), IL = 32 bits&lt;BR /&gt; SET = 0, FnV = 0&lt;BR /&gt; EA = 0, S1PTW = 0&lt;BR /&gt; Data abort info:&lt;BR /&gt; ISV = 0, ISS = 0x00000145&lt;BR /&gt; CM = 1, WnR = 1&lt;BR /&gt; swapper pgtable: 4k pages, 39-bit VAs, pgdp = 00000000b9ddca07&lt;BR /&gt; [ffffffff800005c0] pgd=0000000000000000, pud=0000000000000000&lt;BR /&gt; Internal error: Oops: 96000145 [#1] SMP&lt;BR /&gt; Modules linked in: xxxxx(O)&lt;BR /&gt; CPU: 0 PID: 0 Comm: swapper/0 Tainted: G O 4.19.31-xxxx&lt;BR /&gt; Hardware name:&amp;nbsp;xxxxx based on Freescale S32V234 (DT)&lt;BR /&gt; pstate: 00000085 (nzcv daIf -PAN -UAO)&lt;BR /&gt; pc : &lt;STRONG&gt;__dma_inv_area+0x28/0x58&lt;/STRONG&gt;&lt;BR /&gt; lr : __swiotlb_sync_single_for_cpu+0x4c/0x70&lt;BR /&gt; sp : ffffff8008003cc0&lt;BR /&gt; x29: ffffff8008003cc0 x28: ffffff80006b5000 &lt;BR /&gt; x27: ffffffc03c420800 x26: ffffff80006b5000 &lt;BR /&gt; x25: ffffffc03c420800 x24: 000000000000003c &lt;BR /&gt; x23: ffffffc03c4a7a00 x22: ffffffc03c420000 &lt;BR /&gt; x21: 00000000000005f3 x20: 0000000000000000 &lt;BR /&gt; x19: ffffffc03dd6a0a8 x18: ffffffffffffffff &lt;BR /&gt; x17: 0000000000000001 x16: 0000000000000007 &lt;BR /&gt; x15: ffffff80088c8588 x14: ffffff808892189f &lt;BR /&gt; x13: ffffff80089218ad x12: 0000000000000000 &lt;BR /&gt; x11: ffffff80083c1090 x10: 0000000005f5e0ff &lt;BR /&gt; x9 : 00000000ffffffd0 x8 : 323033203a747075 &lt;BR /&gt; x7 : ffffff80088c85b8 x6 : 00000000000003ee &lt;BR /&gt; x5 : 0000000000000001 x4 : ffffffff80000000 &lt;BR /&gt; x3 : 000000000000003f x2 : 0000000000000040 &lt;BR /&gt; x1 : ffffffff800005c0 x0 : ffffffff80000000 &lt;BR /&gt; Process swapper/0 (pid: 0, stack limit = 0x00000000057e45cf)&lt;BR /&gt; Call trace:&lt;BR /&gt; __dma_inv_area+0x28/0x58&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Code: d1000443 ea03003f 8a230021 54000040 (d50b7e21) &lt;BR /&gt; ---[ end trace 263bcb19fc625165 ]---&lt;BR /&gt; Kernel panic - not syncing: Fatal exception in interrupt&lt;BR /&gt; SMP: stopping secondary CPUs&lt;BR /&gt; Kernel Offset: disabled&lt;BR /&gt; CPU features: 0x0,20802004&lt;BR /&gt; Memory Limit: none&lt;BR /&gt; ---[ end Kernel panic - not syncing: Fatal exception in interrupt ]---&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Nov 2019 13:58:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32v232-with-Linux-Kernel-4-19-31/m-p/1023834#M1491</guid>
      <dc:creator>larry_chur</dc:creator>
      <dc:date>2019-11-21T13:58:23Z</dc:date>
    </item>
    <item>
      <title>Re: S32v232 with Linux Kernel 4.19.31</title>
      <link>https://community.nxp.com/t5/S32-SDK/S32v232-with-Linux-Kernel-4-19-31/m-p/1023835#M1492</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The error means the code&amp;nbsp; attempted a jump or a data access to &lt;BR /&gt;a virtual address for which there was no page table entry. This can happen&lt;BR /&gt;due to multiple reasons, most typically corrupt or uninitialized pointer, memory decay&lt;BR /&gt;or invalid memory size reported by the bootloader.&amp;nbsp; Kernel debugging is &lt;BR /&gt;required to see why and where it fails.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Platon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Nov 2019 08:49:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/S32v232-with-Linux-Kernel-4-19-31/m-p/1023835#M1492</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2019-11-22T08:49:23Z</dc:date>
    </item>
  </channel>
</rss>