<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: using FLEXIO I2C to replace LPI2C function in S32 SDK</title>
    <link>https://community.nxp.com/t5/S32-SDK/using-FLEXIO-I2C-to-replace-LPI2C-function/m-p/993224#M1369</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To change the pins for I2C you have to update pins configuration:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/69497i25B96CD80CCCAE0E/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;After this update FlexIO component with the pins used by your application&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/69674i7E00B09F62032C65/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Razvan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Jan 2020 13:25:55 GMT</pubDate>
    <dc:creator>razva_tilimpea</dc:creator>
    <dc:date>2020-01-14T13:25:55Z</dc:date>
    <item>
      <title>using FLEXIO I2C to replace LPI2C function</title>
      <link>https://community.nxp.com/t5/S32-SDK/using-FLEXIO-I2C-to-replace-LPI2C-function/m-p/993223#M1368</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to use the demo project "flexion_i2c_s32kl46" to read fxls8962's acceleration data( in fact, I can use the LPI2C function to get the data, but the keeping time during reading I2C is not fixed, so I want to try FLEXIO I2C to compare it). I read the demo project's document, and this project uses PA11, PA0 as SCL and SDA. And my S32 board uses the PA2 , PA3. So I want to change the IO configuration in the struct "g_pin_mux_InitConfigArr" from file &amp;nbsp;pin_mux.c . But this does not work. So can you tell me what I need to do to use FLEXIO i2c function to read fxls8962's data? Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yanpo, li&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jan 2020 10:21:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/using-FLEXIO-I2C-to-replace-LPI2C-function/m-p/993223#M1368</guid>
      <dc:creator>yli23</dc:creator>
      <dc:date>2020-01-10T10:21:04Z</dc:date>
    </item>
    <item>
      <title>Re: using FLEXIO I2C to replace LPI2C function</title>
      <link>https://community.nxp.com/t5/S32-SDK/using-FLEXIO-I2C-to-replace-LPI2C-function/m-p/993224#M1369</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To change the pins for I2C you have to update pins configuration:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/69497i25B96CD80CCCAE0E/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;After this update FlexIO component with the pins used by your application&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/69674i7E00B09F62032C65/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Razvan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jan 2020 13:25:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/using-FLEXIO-I2C-to-replace-LPI2C-function/m-p/993224#M1369</guid>
      <dc:creator>razva_tilimpea</dc:creator>
      <dc:date>2020-01-14T13:25:55Z</dc:date>
    </item>
  </channel>
</rss>