<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Trouble updating to S32K1_ISELED_RTM_4.0.0 in S32 SDK</title>
    <link>https://community.nxp.com/t5/S32-SDK/Trouble-updating-to-S32K1-ISELED-RTM-4-0-0/m-p/992838#M1366</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tried installing in the location shown in the image of step 18. It did not seem to work, though the installation said it completed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I go to start a new project from example, I do not see a RTM4.0.0 like I d with RTM3.0.0, or the previous beta versions of ISELED.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Nov 2019 15:32:21 GMT</pubDate>
    <dc:creator>johnathan_weise</dc:creator>
    <dc:date>2019-11-19T15:32:21Z</dc:date>
    <item>
      <title>Trouble updating to S32K1_ISELED_RTM_4.0.0</title>
      <link>https://community.nxp.com/t5/S32-SDK/Trouble-updating-to-S32K1-ISELED-RTM-4-0-0/m-p/992836#M1364</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am having difficulty updating to&lt;SPAN style="font-size: 9.0pt; color: #333333;"&gt;&amp;nbsp;S32K1_ISELED_RTM_4.0.0 from 3.0.0&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.0pt; color: #333333;"&gt;When I launch the .exe to install, I am&amp;nbsp;directing it to&amp;nbsp;the&amp;nbsp;NXP\S32DS_ARM_v2018.R1\S32DS folder, where all the other installations reside, but I don't see a new folder generated when the install finishes I also do not see any new examples when I launch the IDE and try to make a new program. I do see that the ReleaseNotes_ISELED.pdf file is updated to RTM_4.0.0 however.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.0pt; color: #333333;"&gt;Am I directing this to an incorrect folder, or am I missing a step?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Nov 2019 13:49:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Trouble-updating-to-S32K1-ISELED-RTM-4-0-0/m-p/992836#M1364</guid>
      <dc:creator>johnathan_weise</dc:creator>
      <dc:date>2019-11-14T13:49:08Z</dc:date>
    </item>
    <item>
      <title>Re: Trouble updating to S32K1_ISELED_RTM_4.0.0</title>
      <link>https://community.nxp.com/t5/S32-SDK/Trouble-updating-to-S32K1-ISELED-RTM-4-0-0/m-p/992837#M1365</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Johnathan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recommend you to follow the installation guide. Please, see the installation path in step 18. in chapter&amp;nbsp;4. Installation of S32K SDK ISELED driver&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/user-guide/S32K-SDK-ISELED-UG.pdf" title="https://www.nxp.com/docs/en/user-guide/S32K-SDK-ISELED-UG.pdf"&gt;https://www.nxp.com/docs/en/user-guide/S32K-SDK-ISELED-UG.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The available examples are described in chapter&amp;nbsp;&lt;STRONG&gt;5. Examples &lt;/STRONG&gt;in the&amp;nbsp;ReleaseNotes_ISELED.pdf file&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #333333; background-color: #ffffff;"&gt;Which example you do not see?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Nov 2019 15:18:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Trouble-updating-to-S32K1-ISELED-RTM-4-0-0/m-p/992837#M1365</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2019-11-19T15:18:50Z</dc:date>
    </item>
    <item>
      <title>Re: Trouble updating to S32K1_ISELED_RTM_4.0.0</title>
      <link>https://community.nxp.com/t5/S32-SDK/Trouble-updating-to-S32K1-ISELED-RTM-4-0-0/m-p/992838#M1366</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tried installing in the location shown in the image of step 18. It did not seem to work, though the installation said it completed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I go to start a new project from example, I do not see a RTM4.0.0 like I d with RTM3.0.0, or the previous beta versions of ISELED.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Nov 2019 15:32:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Trouble-updating-to-S32K1-ISELED-RTM-4-0-0/m-p/992838#M1366</guid>
      <dc:creator>johnathan_weise</dc:creator>
      <dc:date>2019-11-19T15:32:21Z</dc:date>
    </item>
    <item>
      <title>Re: Trouble updating to S32K1_ISELED_RTM_4.0.0</title>
      <link>https://community.nxp.com/t5/S32-SDK/Trouble-updating-to-S32K1-ISELED-RTM-4-0-0/m-p/992839#M1367</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As the ISELED driver needs to be installed over any SDK RTM 3.0.x so the installation path must be. be&amp;nbsp;NXP\S32DS_ARM_v2018.R1\S32DS\S32_SDK_RTM_3.0.0&lt;/P&gt;&lt;P&gt;The SDK version will still appear as SDK RTM 3.0.0. Please check if the library libiseled_S32K148.a is present in&amp;nbsp;platform\drivers\src\iseled\gcc. If this is the case, the installation was successful, as that library was added in ISELED RTM 4.0.0&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Dragos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Nov 2019 10:34:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-SDK/Trouble-updating-to-S32K1-ISELED-RTM-4-0-0/m-p/992839#M1367</guid>
      <dc:creator>dragosrachitan</dc:creator>
      <dc:date>2019-11-21T10:34:01Z</dc:date>
    </item>
  </channel>
</rss>